Part Number: PGA900 Other Parts Discussed in Thread: PGA302 , PGA300 , , PGA305 , PGA308 , PGA309
Tool/software:
I have some general questions regarding calibration relating to the PGA900, PGA300, PGA302 and PGA305. The main questions are as follows:
What…
Part Number: PGA900 Other Parts Discussed in Thread: PGA302 , PGA300 , , PGA305
Tool/software:
I have some general questions regarding communication relating to the PGA900, PGA300, PGA302 and PGA305. The main questions are as follows:
Why am I having issues…
Part Number: PGA300 Hi,
Q1. Run "Setup_PGA300_EVM.exe", As I proceeded with the process, I got to the "Agree to the license agreement" screen. Will there be additional license fees when using the PGA300 development environment?
Q2 The…
Part Number: PGA300 Hello,
Briefly we have a PT-100 sensor at the temperature input and get voltage output from 0.250 to 4.75 V in our application.
We would like to implement a sensor break diagnostic and for this we have done the following settings from…
Part Number: PGA300 Hi, We configured voltage mode output 0-10V and It works fine for a while. About 3 hours later the chip increase their temperateure and then broke the chip.
The maximum voltage on FB- is 3.6V but Output Voltage is up to 10V. The value…
Hi Scott,
Could you please tell me where 10mA come from in PGA300? not - 2.15V @ 40uS (over limit -0.3V), same token on another end (+10V limit) there is +13.2V @ 25uS, will that hurt PGA300? is there 10mA limit there too?
ESD rating of PGA300 is plus…
Part Number: PGA300 When I calibrated the DAC output of the 4 - 20mA.
Change the DAC output to a higher value, it will cause the PGA300 to be reset as the a higher current jumper (eg. from 3mA to 20mA) when the DAC output is enable due to the resistance…
Part Number: PGA300 Other Parts Discussed in Thread: USB2ANY Hi Scott, we are setting up a production configuration and calibration system for a pressure transmitter using the PGA300.
The system is a Labview application controlling pressure and temperature…
Part Number: PGA300
Hello,
My case is 0-10V and 0-5 psi differential.
1) If I set up DAC HEX 0/1350/2700 related to 0/2.5/5 psi, calibration does not work, WHY?
2) If I set up DAC HEX 5/1350/2700 related to 0.01/2.5/5 psi, DAC calibration works, and calibrated…