Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460 , PGA460-Q1 Hello
We are having issues with distance measurement returning zero FIFO is full of zeros. Power cycling the PGA does not solve the issue. Only solution to this issue we have found…
Part Number: PGA450-Q1 Hi,
we've been reported by our customers that some of our unit's distance measurements are off.
investigation of the fifo data, shows that the echo amplitude is much higher and saturation time is much longer when temperature…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460 Hi,
our company uses PGA450Q1 connected to a waterproof transducer.
this gives us measuring range of >~35 cm up to ~4m.
we would like to reduce minimal distance to ~3cm.
of course, working…
Part Number: PGA450-Q1 Hi,
we've encounter a wired issue using PGA450 in our device.
in some cases, when our device is working at a location with low temperatures (less then 10[C] but more then 0[C]), the PGA450 stops responding to UART requests…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: TIDA-00151
Dear Support,
I have two questions regarding using PGA450 with LIN firmware:
1. Its not obvious for me what is the difference between pre compiled firmware OTP LIN version in output folder…
Part Number: PGA450-Q1 Hello,
Do you have any good in stock alternatives for the PGA411QPAPRQ1? We are having trouble procuring this part and are looking for alternatives.
Thanks,
Adam
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460 Hi Team,
We would like to ask your help regarding our customer's inquiry below.
I am using PGA450 for distance measurement, I have OTP programmed the IC with the Default program. I am…
Part Number: PGA450-Q1 Hi,
After OTP programming the PGA 450 IC, we are able to get the UART response from command 0 (0x12 0x34), but we are unable to get any burst data from Command 1 through UART.
We have verified the SPI EEPROM registers and OTP Programming…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460 , TIDA-00151 , USB2ANY Hi,
Can you help let know if the PGA450-Q1 IC is pre programmed ? Is there any possibility that the default values coming in the OTP and DEV ram can be used for an application…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460 We are using Push-Pull configuration for the burst mode.
How to choose the tdeadtime in the Deadtime Formula(DEADTIME = FOSC × tdeadtime)
the ON_A = 8A (based on the ON_A = dec2hex(FOSC…