Part Number: PLL1705 Other Parts Discussed in Thread: PLL1706 Hello,
I am using the PLL1705 for a system clock of 24.576 MHz at SCKO2. Moreover I am using the Hardware mode.
What should I do with the three-wire interface ML(PIN 7), MC (PIN 6) and MD …
Part Number: PLL1705 Other Parts Discussed in Thread: TAS5753MD , CDCE913 If I have two I2S audio sources configured as slaves driving a TAS5753MD speaker amplifier, is there a simple I2S "controller" IC that can generate the SCLK and LRCLK to all three…
Other Parts Discussed in Thread: PLL1705 Hello! I solded my PLL1705 on a adaptor board and connected it to the breadboard, connections had already been checked and there is no fault, the circuit is properly connected with a 27MHz crystal.
however, when…
Other Parts Discussed in Thread: PCM1792A , PLL1705 , TMS320F28335 Hi,
my
design is based on F28335 microcontroller, which provides PCM1792A DAC
through McBSP serial port with serial PCM data. I wanted to use PLL1705
to clock both of those devices. However…
Hi Eric,
Do you have requirements on the clock jitter? Do you need all thee frequencies simultaneously? Or any other requirements?
You may be interested in an audio clock such as PLL1705. PLL1705 can generate one of these frequencies at a time on SCKO2…
Hi Trieu,
Neat looking PCM1808 module you found there! Take a look at Figure 3 in the PCM1808 datasheet - if SCLK is not present (fixed to high or low), there will be zero DOUT.
If you are really using a 12.288MHz crystal soldered between GND and SCK,…
Part Number: AM5708 Other Parts Discussed in Thread: PCM1681 , , PLL1705 , BEAGLEBOARD-X15 , AM5728 , TMDSEVM572X , TMDSEVM437X
Tool/software: Linux
HI all:
We have connected the pcm1681 to am5708's mcasp2。
We used pll1705 to provide the clock to am5708…
Part Number: TMS320DM6437 Other Parts Discussed in Thread: PLL1705 I can't understand the concept of Audio PLL/VCXO Circuit/PLL1705 Clock Generator while reading the tech reference manual of DM6437.Please explain the concept clearly
Other Parts Discussed in Thread: SRC4192 , PLL1705 Dear Sir
i have tested SRC4192 evaluation board and get below observation
Setting
1. 16bit 44.1K signal input from SPDIF to CS8414 BCLK, data, LRCLK to SRC4192
2.SRC4192 clock source by PLL1705 with 24…
Other Parts Discussed in Thread: PCM1801 , PLL1705 Hello everyone, I ran into some issues while working with the PCM1801 16 bit Stereo ADC (Datasheet: http://www.ti.com/lit/ds/symlink/pcm1801.pdf ) The chip was set up as show on page 17 of the datasheet. The…