Hello Kersten,
The LM3481 is capable of working under your conditions. Look up PMP10610 at www.ti.com/.../PMP10610 to get started. Increase the voltage of the input and transfer capacitors by 20 V and use either 80 V or 100 V MOSFETs. The output current…
Thanks Dileep for sharing the details of your design .
Below are some points on Schematic ,layout and the ways you can debug the radiated EMI issue .
Schematic:
Can you please let me know why are you using both an uncoupled inductor L4 and a coupled…
Hi Pablo ,
Please find below the comments on rhe layout :
1. Caps at Vin and Vcc need to be placed next to IC pins and IC GND .
2. THe high current path is laid out properly but high switching curent output loop needs modification :
3. Please…