Part Number: PMP11281 Is PMP11281 design still valid and ready for wall mounted USB adapter /charger application or it has any problems , I want to use it in my new product (4 ports USB universal adapter/charger 2.4A each). it will be connected all the…
Other Parts Discussed in Thread: UCC28630 , UCC28730 Finished the design of a power supply of (ucc28630) 12V 65W, this uses a diode rectifier output
We are evaluating the design of a 65W 5V.
In the schematic PMP11281 (ucc28730 5V 50W) uses a synchronous…
Lanhua
I assume that this is for universal AC input (90-264 V)?
There are several reference designs on the UCC24630 product page, click on the "tools & software" tab.
www.ti.com/.../toolssoftware
There are some 5-V high output current…
Hi Amit,
While it is certainly possible to design a flyback with 8A output, this would not be the design to use as a starting point.
The transformer would need to be completely changed.
The output rectifier needs to be synchronous instead of a diode. …