Part Number: PMP20588 I am using PMP20588 reference design. It is working fine. I want to use this DC-DC converter section for 54VDC, 2.5A output . Is it possible with this device? If yes,please suggest me the required changes in the present schematic…
Hi Mortiz,
Customer referred a similar reference design PMP20588 and the transformer Pri: Sec is 1:5.
The transformer customer used Pri:Sec PL3254-001SR_SPEC_A.pdf is also 1:5(not 1:1).
Could you please review again what might be wrong?
Thanks,
Allan
Part Number: CSD19538Q3A Other Parts Discussed in Thread: TIDA-00290 , PMP20588 , TIDA-01411 Dear All,
there a numerus different design from TI on how to protect PSE mosfet, which one is the most recommended one?
1) No protection eg: PMP20588, TPS23861EVM…
Hello,
We would recommend one of our single port PSE designs, but they use a newer part.
The TIDA-00465 uses a 54V DC input and an LDO to get the 3.3V rail.
https://www.ti.com/tool/TIDA-00465
The PMP20588 uses a 12VDC or 24V AC input which is then…
Part Number: TPS23881 Other Parts Discussed in Thread: PMP22764 , PMP20588 , , BOOST-PSEMTHR-007 , PSEMTHR24EVM-081 Dear All,
we are designing PoE PSE 802.3bt Type 3 Class 5 45W single port
1) I was going through many TI PSE designs, and the PSE output voltage…
Part Number: TPS23861 Other Parts Discussed in Thread: PMP20588 Hi TI Team,
We are using TPS23861 PSE controller in one of PoE/PoE+ application to switch 54V to the PoE device.
During temperature measurement I can see the delta temperature for this IC…
Other Parts Discussed in Thread: PMP20588 , LM5022 , TPS23861
This is a schematic drawing that fully refers to TI's reference design, TI's drawing number is PMP20588.Web link: www.ti.com.cn/.../PMP20588
The change is that the transformer is changed…
Part Number: LM5022 Other Parts Discussed in Thread: LM5155 , LM5156 Hello everyone,
We are going to design a carrier board have 4 port GbE with PoE-PSE (all ports support 802.3 bt 30W out),the input power is 9~36V DC,the PSE Controller is TPS23861PWR,i…
Part Number: TPS23861 Other Parts Discussed in Thread: PMP20588 Hi Sir,
TPS23861 is support four ports, can suport two ports? how to design it? is there reference design, thanks.
Hi Gareth,
Thank you for your questions.
On the PSE side, we don't have a single port only PSE but the TPS23861 is recommended for single port up to 30W PSE applications. You can find a reference design PMP20588 where the TPS23861 is used in a single…