Part Number: PMP20859 Other Parts Discussed in Thread: TPS2372 Hi,
I would like to ask why R35 is configured to 27.4k ohms? This contradicts the TPS2372 datasheet which recommends 24.9k ohms.
Thank you,
Sith
Part Number: PMP20859 Other Parts Discussed in Thread: TPS3808 , TPS2372 , TPS2373 Hi Experts,
I have a few questions regarding this design:
Why is there a need for the UVLO of the converter to be pulled low by Q9? I thought that unless the inrush…
Part Number: TPS2373 Other Parts Discussed in Thread: TPS2378 , TPS2372 , PMP20859
Dear Team,
Below redundant PD is for .bt, if I want to implement .at version just change the TPS2372 to TPS2378, right?
Or you have better total solution or reference…
Part Number: PMP20859 For PMP20859,
I see the R58 package for 35.7kohm is 0603 on PMP20859, but it's only 1/16W.
Is it ok?
Please help to check how to calculate it?
Part Number: PMP20859 Other Parts Discussed in Thread: TPS2373 , Hello Sirs,
Just need to double check this PMP20859 .(two tps2373 + single isolation flyback )
Is it no problem for two PSE input redundant power input , and system still working without…
Part Number: PMP20859 Other Parts Discussed in Thread: TPS2372 What are the benefits of using TPS2372 (PoE High-Power PD Interface with Automatic MPS & Autoclass) in the implementation of a “smooth transition” PoE PD reference design?
Part Number: TPS23754 Other Parts Discussed in Thread: PMP20859 Tool/software: Hi Sir,
if i want to switch between DC adapter and PoE , i need hotswap without reboot. how to do it?
the current approach is to give DC priority and will restart once…
Part Number: TPS2373 Other Parts Discussed in Thread: PMP20859 , PMP22477 Hello, when developing wireless APs on the Qualcomm WiFi7 platform, we selected the following (PMP22477/PMP20859) 2 bt_PD reference designs from TI for a variety of different product…
Part Number: TPS2372-4EVM-006 Other Parts Discussed in Thread: PMP20859 Q1:If I use the FDMQ8205A(ideal diode bridge) in the TPS2372-4EVM-006, how does the FDMQ8025A block reverse current to each other?
e.g, if the signal pair input is +57V, and the…