Part Number: TMS320F280049 Other Parts Discussed in Thread: SYSCONFIG , PMP23069 Hi champs,
My customer is studying PMP23069 reference design, he finds that he can use sysconfig file to add peripherals, for example SCI. However, he cannot configure the parameters…
Part Number: PMP23069 Other Parts Discussed in Thread: CONTROLSUITE , TIDM-1022 Hi,
My customer wants to test C2000 solution on their existing product(bridge, CCM, single phase PFC + competitor MCU).
-110\220VAC to 400VDC\380VDC
-1Kw output
-CCM
-need…
Hello Sandra
One way is to start with epwm example project of F28379D in C2000ware. Once it is running, try importing the project file of pmp23338 in this project.
Better than C2000ware project, you can refer TIDM HV DC-AC (implemented both on F28379D…
Part Number: TMS320F280049 Other Parts Discussed in Thread: PMP23069 , PMP23338 , PMP40988 Tool/software: Hello, I want to implement PLL (Phase locked Loop) on F280049 to synchronising grid connected inverter with grid voltage. I was wondering if there is…
Hello Xinghang
SPLL is used in PMP23069 reference design to compute the phase of input AC signal. You can find the code of PMP23069 in digital power SDK, solution folder. Please download the latest digital power SDK from TI website.
Thanks
Amir
Hi Amir, thanks for the reply. I looked through the reference design for pmp23338 and pmp23069 whiles writing this code and i looked at the pll part and did the same. I am a bit confused because that code is a whole state machine and I picked out the…
Part Number: TMDSCNCD280039C Other Parts Discussed in Thread: PMP23069 Hi TI support
I am working on PMP23069 TI example code to run our new board design.
I have question regarding the current sense calibration and calculation, I am not able to understand…
Part Number: PMP23338 Tool/software: Hi,
I am trying to get the inductors for this reference design and I cannot locate them.
In a similar thread
https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation…
Hello Amir,
This is PMP23069 referance design. But it perform with average mode current control. I want to use the peak current mode control. Also my circuit is 2 phase interleaved.
Thanks,