Part Number: PMP9053 Hi all,
I tried to follow the power supply reference designs, PMP 9053 and PMP 9608. These two designs are very similar. PMP 9053 outputs 3.3V while PMP 9608 outputs +-3.3V. However, I found the diodes used for PIN 1 and 2 of transformers…
Stephane
The specs for transformers like this are the intellectual property of the transformer manufacturer. TI cannot publish the specs without permission.
Sometimes the specs are available from the transformer manufacturer website, you should check…
Hi Ehsan,
You could use full-wave rectifier (example: PMP12082) or half-wave rectifier (example: PMP9053) for 3 phase input. 24V 1A is quite high power for a AC-DC buck converter. Especially if you are using UCC287xx PSR controller in Buck converter topology…
The Smart Plug design actually uses a single phase version of pmp9053 ( http://www.ti.com/tool/pmp9053 ).
The transformer is a Renco RLTI-1094. You can contact Renco on engineering@rencousa.com
Hope this helps.Thanks,Billy
Hi,
I'm looking for some references, applications notes and schematics to design a power supply for a RF devices.
The main specs for applications are:
Vin: 230V AC single-phase
Vout: 3.3V DC
Iout<100mA
I have seen that this TI flyback converter…