Part Number: LM5022 Other Parts Discussed in Thread: PMP9334 , PMP20196 , Hi
I have seen reference design PMP9334 and PMP20196 using of LM5022.
I am starting Low Wattage SMPS design I have some question for this LM5022 on below
1. Solution -1
Input -15V…
Part Number: PMP9334 Other Parts Discussed in Thread: TINA-TI , , LM5022
Tool/software: TINA-TI or Spice Models
Hi
Anybody has done the simulation of PMP9334 design in any software.I want to increase the input range of design to 19VDC to 380VDC.
Other Parts Discussed in Thread: PMP9334 Hello~
According to the BOMs of PMP9334, Transformer's part no. is " G094215LF " of GCI Technologies.
30 to 300Vin to 15V@1A Output High Voltage Flyback Converter Reference Design (ACTIVE) PMP9334 http…
Other Parts Discussed in Thread: PMP9334 Hi All,
Please let me ask about PMP9334 reference design.
In this design, the auxiliary winding is divided and input to FB pin. Please let me know the purpose of this configuration. I'd like to know the operating…
Other Parts Discussed in Thread: PMP , LM5022 Dear TI
Custoer has question for PMP schematic on below URL.
http://www.ti.com/lit/df/snvr397/snvr397.pdf
There are diodes of D103and Z1 in 1st trans side and they are DNP.
Customer would like to know what case…
Part Number: TPS40210 Other Parts Discussed in Thread: PMP9334 , I've a requirement for SMPS as below:
Vin range: 30-350V
Vout1: 18V @0.7A
Vout 2: 12V @0.5A
Fsw: 85-100KHz
Topology: Flyback DCM
Isolation: NO
Cout: 56.2uF
I've taken feedback from 18V…
Other Parts Discussed in Thread: PMP20745 , PMP9334 Dears:
There is a demand as follows:
1. DC-DC input is 18v~380v, output is 12V or 5V
2. Iout is 1.5A or 2A above.
I found the solution from reference design.
And from the PMP20745 datasheet I can see…
Part Number: LM5022 Hi I have a question about the schematic the used for the Isolated Flyback Converter. In the schematic they use the G094215LF transformer from GCI Tech. The problem is that I cant find any Datasheet to this transformer. Does anybody…
Part Number: LM5022-Q1 Dear all,
I'd like to find the right values for the resistors RSNS, RS1 and RS2 in regards to current limiting with taking the slope compensation into account. The formulas in the datasheet of the LM5022-Q1 on page 21 are for…
Other Parts Discussed in Thread: UCC28700-Q1 , UCC28700 , LM5022 , PMP9334 Hello, For a new project, we have to design an isolated DC-DC power supply.
The minimum requirements for our project are: Input: 9Vdc to 60Vdc Output 1: 5Vdc ±5% @ 2A Output…