TI's tech support pointed me here to determine if they do or do not support pin-in-paste for this power module.
Does anyone have any insight they can share? I have a large build coming and need to streamline in a hurry!
Thanks,
Ed P (noob) …
Hi Carlo,
It seems customer has asked the same question on the below thread.
https://e2e.ti.com/support/power-management/f/power-management-forum/997443/pth08t230w-thermal-resistance-rj-for-the-device
We will response on the other thread. And this one…
Shruti:
PTH08T230W EMC/EMI conducted and radiated emission Data is attached.
EMC is conducted reference data . The PTH08T230W requires input PI filtering to achieve fore conducted and radiated emissions . The input Ferrite bead ( # is 2773021447 Fair…
Thank you, that is what I suspected - but had the LDO pull a lot of current for some reason.
Turns out the customer had a PTH08T230W connected to the same rail, that was also enabled - the switcher was trying to regulate and pulling the rail down!
Disabling…
Hi,
We spoke about my power application a few weeks back.
You had offered to give us our average power figures based on the voltage drop across the inductors.
Here are the modules we are using and the voltage drop across the inductors and temperature…
Other Parts Discussed in Thread: PTH08T230W , PTH08T220W , PTH08T250W Hello there,
We are using PTH08T230W, PTH08T250W and PTH08T220W in our board.
We need to design heat spreader for our board and we need the exact height of the modules (from the PCB to…
Chandana Bhat :
I reviewed section 1 and section 2 for Turbo trans (Rtt=0Ω) .
Section 3 has a comment about the output ceramic capacitance required for PTH08T230W
Section 1 .The capacitance with low ESR>10mΩ( 25A current step ) 8298uF 13…
Alexandre:
I suggest the PTH08T230W for this application. Average input current at 5V5 is about 75mA with 12Vin . The component temperature at no load is about 49°C.
Tom
Other Parts Discussed in Thread: PTH04T240W , PTH08T230W Do TI has another power supply structure for XC5VLX85 FPGA excpet using PTH04T240W, PTH08T230W modules?
Thanks.