Part Number: PTH12050W Hi Team,
My customer is looking for the 3D/step file of PTH12050W
If available, can you provide the the file to us?
Thank you.
Regards, May
Part Number: PTH12050W If the POLA Regulator parts PTH12050WAD and PTH12050WAH are now mechanically and electrically "equivalent' why does TI still offer both options ? Producing both versions must have a cost associated. Is there an advantage to offering…
Part Number: PTH12050W The 12V supply voltage to this module has instances where it will temporarily go as high as 14V for a period of 1ms.
This spike is outside the maximum voltage for this part of 13.2V. Since it lasts for a small duration when it occurs…
Part Number: PTH12050W Other Parts Discussed in Thread: LMZ31506 , LMZ31707 We use these Texas Instruments DC-DC converters in multiple designs. The PTH12050W is used to convert 12V down to both 3.3V and 1.2V.
Issue we are seeing is that the modules that…
Part Number: PTH12050W
Hi,
"SLTA055 - Februrary 2006" application report is a great app-note but, it's only apllying to single-phase, isn't? if so, is there a version for multi-phase e.g., 2 or 6 phases design?
Thanks,
Tim
Part Number: PTH12050W Using PTH12050W with Vin = 12V, Vout set for 5V or 3.3V. Track pin is tied to VIN and Inhibit pin is unconnected.
When the module is powered up with zero load or near zero load, a glitch in the output is seen after about 18 ms,…
Part Number: PTH12050W What is the difference between a PTH12050WAD and a PTH12050WAH and where in the data sheet does it spell this out?
What is the difference between a PTH12050WAS and a PTH12050WAST and a PTH12050WAZ and a PTH12050WAZT and where in…
Other Parts Discussed in Thread: PTH12050W Hi All,
I am unfamiliar with our Power Modules and wanted to ask a question with relation to the no load current.
If the PTH12050W is supplied with 5V and there are no caps input or output, would the 'Input standby…
Other Parts Discussed in Thread: PTH12050W , PTH12060W I'm working on a power distribution design which is heavily based on previous generations in which I'm using the PTH12050W to generate one of the low current rails (<5A). I would like to add…