Part Number: BQ78350-R1 Other Parts Discussed in Thread: BQ76940 , , BQSTUDIO
Hello I am using bq78350-r1 and bq76940. I am reading SMBUS data using sbs commands with MCU . I can Read in SEAL MODE the total voltage, cell voltages, temperature and similar values…
Hello Matej,
The bq evaluation software for bq27000 was shipped on CDs. There is no downloadable link.
If you can debug your issue by logging SBS data, then you can download any other bqEVSW and select a SBS compatible device, then go to SBS and select…
Part Number: AWR2243 Hello,
When I was debugging the AWR2243 single chip, I found that the startup process printed out: MSS CPU Fault
I want to figure out what exactly went wrong. How can I print the specific error types of MSS CPU Fault? Here are some…
Part Number: BQ20Z95
Hi Community Members,
We use bq20z95 in our project. SBS commands return us correct values. However, extended sbs commands do not return correct values.
We tried to check which mode the bq20z95 is in with "OperationStatus (0x54)"…
Hello
I am trying to compile the soundbar code and I am getting the following error. I am using the latest version of IAR workbench.
Any help in getting this error resolved will be great.
Thanks,
Subbu
Building configuration: SoundbarCode - Debug Updating…
Part Number: AWR2243
Hello,
I would like to ask, when we cascade the AWR2243 chips, we use a phase shifter. When calibrating the phase shifter, we refer to the article "Cascade Coherency and Phase Sifter Calibration Application Note". We plan to use…
Okay, so since SBS Voltage is a present value with respect to the bat terminals we would be decrementing AvailableEnergy during discharge by less than what is true since the voltage sags during DSG. This would lead to the outward bend of the curve over…
Hello Jason,
You can pull some of the information with the SBS register in the gauge, which can extracted while the gauge is sealed or unsealed. To pull the Ra table values you would need to unseal the device to extract the tables from dataflash. We recommend…
Hi Dhaval,
Thank you for reaching out.
1. There is only a slight difference. For example Rvs1 is 58k as per the formula in datasheet. Whereas the one in excel sheet optimizes based on available resistor values. It is there in a sheet titled "LOOKUP TABLES…