Hi
I have Requested Friendship so we can talk in private message to keep info secured.
I do not find the above order in our production system was this a test order or a prod order you are wanting to simulate.
I also do not recognize this form- at the…
Part Number: REF3033 Dear Sir,
We photographed the lead frame design for counterfeit testing of the REF3033AIDBZR.
Fig 1. shows the lead frame design of REF3033 with CoC (Certificate of Conformance).
Fig 2. is the lead frame design of REF3033 without…
Part Number: REF3033 Other Parts Discussed in Thread: OPA310 , LMV861 , TLV341 Hello,
1. is there a way to increase current drive by adding an external transistor? if yes, please recommend the circuit
2. IS there any alternate part which is similar with…
Part Number: REF3033 Datasheet, section 9.1 clearly stated that output cap is not required.
It does have a clause in section 9.1 for "special care when using low ESR caps and high capacitance"
Is there a guideline on what is "low ESR"? What…
Part Number: REF3133 Other Parts Discussed in Thread: REF3033 , , REF20-Q1 Hi,
The REF31xx datasheet lists +/- 10 mA as the current rating, but then in 7.3, Recommended Operating Conditions, it lists 20mA. Is that a datasheet error, or can this part ac…
Part Number: REF3033 Hello all,
in my Design I use the REF3033 for Mikrocontroller ADC-Reference Voltage (VDDA33). There is a permanent minimum current of 3.3mA at "OUT"-Pin.
I also have an Analog Input Pin (Ana_IN1) at my µC. To protect the…
Part Number: REF3033 Hi team,
I have a question on the REF3033 datasheet regarding to the accuracy description.
One page 1 of the data sheet, there's a curve of output voltage VS load current. And in Figure12, there's also a curve on that. The two curves…
Part Number: REF3033 Hi team,
I'd like to confirm below 2 things.
1. the datasheet mentioned Dropout voltage is 50mV max in TA=25C, Iload=0mA. Could you tell me how much the Dropout voltage when Iload is 25mA during -40 to 125C?
2. How much the…