Part Number: REF5010 Hi Team, we are looking for the "voltage noise for each member of the REF50xx family" on the datasheet.
Hoping for your inputs.
Thank you.
Regards,
Mark Felipe
Part Number: REF5010 Hi Team,
One of my customers connects the circuit according to "Figure 42. Basic Connections". Input voltage is 12V but the voltage output of pin 6 is just 7.7~7.8 V. Could you give me some advice?
Beat Regards, Tom Liu
Part Number: REF5010 Dear Sir,
We are planning to use REF5010ID and REF5050ID in our existing design.
In view of the above we want to know the end of life of the product.
Regards,
Arun P
Part Number: REF5025 Tool/software: I'd like to use this to create a -2.5v reference (as well as another one for -12.5v reference, stacking a REF5010 and a REF5025). App note SBOA362 (Low-Noise Negative Reference Design with REF5025) does not show…
Part Number: REF5010 Hi team,
Customer is using REF5010, but under some case, there may have 20mA current flows into the Vout of REF5010.
Will this cause permanent damge to REF5010 or not?
Customer can't use doide to prevent the reverse current because…
Part Number: REF5010 I'm using a REF5010 precision reference and a OPA189 op-amp to create a precision current source to excite a bridge in a pressure sensor, please see attached TINA-TI simulation schematic. In the REF5010 data sheet, SBOS471B-APRIL…
1. There is no similar device in the TO-5 package. The nearest replacement would be the REF5010.
2. There is no similar device with four-channel AND/NAND inputs. The nearest replacement would be the SN75159 with two inputs each, and a different pinout.…
Part Number: REF5010 Hello,
I have to design a 10v@100mA precise reference with REF5010. But REF5010 can provide only 10mA current. I have modify the circuit for current boost. Simulation are good. Circuit diagram and simulation is also attached. All…
Hi Tony,
I looked into it more and tested a few devices. The output on the trim pin and the output on the reference pin are consistent across all of the devices, but it does vary with the expected value as reported in the datasheet, as you discovered…
Hi Naga,
From your specification, the input strain gauge is operated between 349.5Ω and 352Ω range. I selected INA818 instrumentation amplifier (IA) for the analog front end. The IA amplifies mV signals to V signals for the XTR111's V-to-I conversion…