Part Number: REF6025 Tool/software: I am reaching out to request Coefficient of Thermal Expansion (CTE) data for the components above. Could you please provide us with the CTE values ? We would appreciate it if you could provide the CTE values in ppm…
Part Number: REF6025 Tool/software: Hi experts,
For the output capacitor of REF6025, customer prefers two types: 22uF, 80mohm ESR electrolytic cap, or 47uF, 45mohm ESR, electrolytic cap. However, for 22uF cap, the ESR may drift to as high as 160mohm…
Part Number: REF6025 Other Parts Discussed in Thread: REF60 Tool/software: Hi experts,
For the output capacitor of REF6025, customer prefers two types: 22uF, 80mohm ESR electrolytic cap, or 47uF, 45mohm ESR, electrolytic cap. However, for 22uF cap,…
Part Number: REF6025 Other Parts Discussed in Thread: ADS8887 , , ADS8881EVMV2-PDK , ADS8881 , REF6045 Tool/software: I am using the REF6025 and ADS8887 in a design, with the REF6024.
The datasheet for the REF60xx series, on page 23, in section 9.3…
Part Number: REF6025 Hi,
I'm looking to use the REF6025 and was looking at the SS pin to maximize the current.
On the pin configuration and functions section it says "Connect to Vin pin for highest current limit", is this a short connecting SS to…
Part Number: REF6025
Dear Sir, please answer
I asked a question about REF6025 in Jun 2017. Please see my circuit in attach.
I need to adjust frequency of generator - 16,384,000 Hz. I need to vary voltage in the generator's control input "VC" in…
Part Number: REF6025 Dear Sir, please, answer
I'd like to use REF6025 for voltage control of Voltage Control Oscillator JT53LV (16 MHz) . Oscillator has control input for feed 1.5 V+/- 1V voltage. I want to adjust this voltage with a potentiometer,…
Part Number: REF6025 Other Parts Discussed in Thread: ADS1259 Hi,
I apologize that this topic is not related with the REF6025 directly.
Please move to proper forum if this forum is inappropriate.
I watched the delta sigma-voltage reference training…
Part Number: REF6025 Hello,
Our customer has a question for REF60xx. There is Figure 17 and 18 (see below) for load transient response in the datasheet(SBOS708B). What is C_L value for these graphs?
Regards,
Oba
Part Number: REF6025 Hi,
three questions regarding REF60xx:
1) Does the yellow marked text refer to CFILT or to CL? (Can the ESR of CFILT really have a noteable impact on the stability as it isn’t a conventional OP/buffer)
2) What is the value of…