Part Number: REG71050 1) What is the maximum power dissipation value for the various packages?
2) What pin, if any, is the exposed thermal pad connected to on the DRV package?
3) The thermal resistance to the board seems to be lowest on the DBV package…
Other Parts Discussed in Thread: REG71050 Hi,
My customer has question about REG71050. Could you tell me about questoin?
[Question] - My customer considers to use small size Cpump than recommended value. It is under the below.
Cpump= 0.22uF 1005size 10V …
Is it possible to connect the thermal pad to Vin ?
Due to optimized layout this is a practical consideration.
Is there an electrical connection from thermal pad to die attach ?
Other Parts Discussed in Thread: REG71050 Hi,
My customer has question about REG71050. Could you tell me about questoin?
[Question] My customer considers to use EN pin pull up to Vin. Is there any consern about this usage?
Best Regards, tateo
Other Parts Discussed in Thread: REG71050 , REG71055 , REG710-5 Let me ask about REG71050.
Is the input voltage range of this IC 2.7V?5.5? I contributed, in order that there might be no statement in a data sheet.
yusuke
Other Parts Discussed in Thread: REG71050 , TPS60150 Support,
Customer needs tigher regulation from the REG71050. 4.7V to 5.5V is too wide. If there was a way to make the regulator regulate to the higher voltage that would be better. Is the any way to do…
Gabriele,
The delay time before the charger changes from charging with power applied at VBUS to boosting from the battery to PMID is fixed and cannot be changed or shortened. Can you add a simple circuit that senses when VBUS is removed and quickly puts…
Part Number: TLC59731 Other Parts Discussed in Thread: TLC5973 , , LM3699 , REG71050 , TPS60231 Hi,
I'm looking for some help setting the current for each channel of this device. If I want to supply my device with 3.3V and my blue LEDs have a Vf of 2.8V at…
Juha-san,
Thank you for your reply. And our customer input voltage was change. Their latest requirement is Vin=3.3V, Vout=-5V, Iout=30mA, Height is lower than 1mm.
Do you have any solution for their requirement?
I think they should use REG71050 and LM27761…