Could you please try the following:
1. Download the file attached. Change the extension from .txt to .bin
2. Run it from the command line with the following parameters:
"ti_simpack_vayu_ccs_0.6.2.0_setup.bin" --mode silent --prefix "/home/vasanthaangappan…
Hi Stefan,
I've attached the zImage and the modules for the corresponding image. Please try this out and let us know if it works. Copy the zImage to the boot folder in the rootfs partition and the modules to the lib/modules folder in the rootfs partition…
Hello Hideaki,
I'm not too familiar with these labs, but I do have a couple of BIOS examples for F28377D that use controlSUITE. These examples use IPC to send messages between CPU1 and CPU2, though, which may be more than what you are trying to do…
Hi Vivek,
I have C6000 Labs and Solutions. I'm not sure if they were meant for the OMAPL138 or not. The comments in the code say '6748 EVM'. I will post them so you can have a look.
Best regards,
Janet
2477.TI_RTOS_Labs_and_Sols_C6000.zip…
Hi Patrick,
nothing is wrong, we found out an unexpected bug in the software. The correct version will be updated by today on the website. In the mean time I can share with you this version in advance. Could you please try it out and check if you face…
Wojciech,
The attached v0.9.65 installer should have all the required files. I already tried to attach it as an exe, but it was rejected. So, the attached file has its extension changed from exe to txt. Just change it back and run it.
Regards,
Dou…