The temperature range is from 25-45C. I need to modulate the current at a minimum of 80MHz, ideally to 180MHz to achieve multilevel laser pulses. Is there any alternative IC or workaround that you could suggest, since it seems that this is beyond the…
Part Number: AWR2243BOOST Other Parts Discussed in Thread: AWR2243 Hi, I am using the AWR2243/AWR2243 BOOST 4-chip cascade radar for some tests and I have successful processed the captures for range-azimuth and range-doppler visualizations. Then, I checked…
Part Number: TUSB1210-Q1 Tool/software: Hello, I have a question about estimating the maximum current consumption for components, both at typical and heightened temperatures
I am currently designing a circuit that is required to operate at extended…
Hi Rannie,
I have a few questions,
#1 - the data sheet of the post stage shows a 7-inch display which includes MIPI interface, set for this resolution: 1024 x 3(RGB) x 600.
This seems different than the TAP HMI 2.1" 480 x 480 on the block diagram…
Hi Mike,
mmWave Sensing Estimator (v2.4) doesn't support AWR2944 and there is no tool similar to this which can help you with the RF configuration. Refer to "C:\ti\mmwave_mcuplus_sdk_04_06_02_01\mmwave_dfp_02_04_16_00\docs\mmWave-Radar-Interface-Control…
Hello Kei-san,
There is a difference between RF range and RF bandwidth. For example, the above interpolation ratio with 4GSPS DAC will support about 300MHz of bandwidth (interface bandwidth between customers digital ASIC to our DAC). The customer may…
Hello O.H
The CC2592 is a RF front end Range Extender , I assume you already have another device attached to the CC2592 and that device is using DSSS (ZigBee?).
Quoting another response to DSSS on another thread:
"DSSS is included in Z-Stack kernel…
Hi Kazuya,
Kazuya Nakai59 said: V'CS = Vout((RF+RCS)/(ROFF+RF+RCS)
As the result of calculation with each VOUT, they found 15.657mV difference between each VOUT case, 20V and 50V.
They think 50V case output current is lager 104.38mA(15.657mV/RCS…
Hi,
I suspect that the Target I2C address value located in the DEVICE_CONFIG1-> I2C_SLAVE_ADDR register may have been modified. Are you receiving NACK responses across the entire I2C address range (0x00 to 0x7F)?
This is the reason I recommended using…