Hi Fong,
Fong Zi Hao said: For the sensing estimator, using the same parameters shown above but for AWR1843BOOST, the maximum range turns out to be 76m which is lower than AWR1843AOP (107m), is this normal? I was expecting a longer range on the BOOST…
Part Number: AFE8030 I intend to use the AFE8030 octal transceiver. The RF ports impedance is not given in the datasheet. Only that it has -12dB return loss with matching. There are some examples for 700MHz and 1800MHz, but I want to use it at different…
Hello Kuwahara-san,
Using the propagation delay as a good estimate, typical data rate would be 400Mbps or 200MHz.
Data rate is determined by temperature and output voltage meaning 500Mbps cannot be supported across all voltage ranges.
Regards, …
HI Sima, Thanks a lot for the data provided. Using the default datasheet configuration means: VS = ±5V, RL = 100Ω, and RF = 237Ω, isn't it? Also as far I saw in Michael's work, in another e2e thread to estimate the OPA695 noise at low frequency (< 1kHz…
Part Number: ADC32RF55EVM Other Parts Discussed in Thread: ADC32RF55 Ti team,
We have procured the ADC evaluation board for the ADC32RF55 (Dual Channel, 14-bit, 2.6–3 GSPS RF Sampling Data Converter).
We have a few clarifications regarding its operation…
Part Number: AWR1843BOOST Tool/software: AWR1843BOOST OOB Demo – Range drops when ego vehicle is moving
Hi,
I'm using the AWR1843BOOST with the Out of Box demo. While testing on a moving vehicle, I'm seeing that the detection range drops from…
Part Number: TMUX6234 Hello,
I am currently designing a circuit which drives switching inputs for an RF switch. These inputs require either appr. -30 V or 0 V, so I found wiring the TMUX6234 to -30 V and 3.3 V to be a suitable solution for controlling…
Part Number: REF54 I am using the REF54 voltage reference in my design, specifically the 4.096V part REF54410. In the datasheet for the part on page 3, there is a device comparison table in which, according to the footnotes, only the SOIC package C grade…
Hi Amarnath,
We do not have any thermal models available for TPS65220.
We do offer a Thermal estimator tool for TPS65219, a device in the same family. This will also give a good estimation of the thermal information for TPS65220x devices, but keep…
Hi Dmitry,
HWA FFT engine has a pre-processing block which performs interference localization to identify samples corrupted by interference followed by interference mitigation to repair those samples. Any sample whose magnitude and/or magnitude of backward…