Part Number: LMV931-N Hello,
This is a follow-up to our previous thread regarding the LMV931-N input offset voltage.
In the previous discussion, it was mentioned that the LMV931-N has a typical input offset voltage of ±1 mV, with a maximum of ±4 mV…
Hi Teritama,
Here are my responses to your questions -
1. Vio is offset voltage as mentioned in datasheet on page 7.
2. Certainly, error-amplifier of the UCC2895x is not characterized as Zero-TC or PTAT or CTAT type.
3. ±1uA is the absolute max…
Part Number: TPL7407L Other Parts Discussed in Thread: AM263P4
Hello,
I am using the TPL7407L as a low-side driver for a 24 V digital output signal, and I need to estimate its switching times in my configuration.
Configuration: - Device: TPL7407LAQPWRQ1…
The thread above already shows how to verify stability by simulating phase margin (minimum 45 degrees) and confirming stable operation with small-signal transient analysis (max 25% overshoot). As far as procedure goes, first, you need to determine the…
Hi Umesh,
The DRV2511-Q1 is AEC-Q100 Grade 1 qualified for an ambient operating temperature (TA) of –40°C to 125°C. Please refer to the datasheet Features section and the orderable part information for DRV2511QDAPRQ1, and it is the range listed on the…
Part Number: AFE7903 Dear Team,
We are using AFE7903 in our design.The device is been used for the frequency range of 4.4GHz to 5GHz(600MHz BW).
As per datasheet's RF ADC Electrical Characteristics the gain flatness is mentioned as 1.1dB for 400MHz…
Part Number: AWR1843AOP Other Parts Discussed in Thread: AWR1843BOOST , AWR1843 , AWR2944
Hello,
We are currently working on AWR1843AOP for one of the ADAS application. We have a desired detection range of 100m and above and by changing the initial…
Hi Xie,
1. Understood the occurrence of problem is random, but would like a general estimate. Is it within the range of 1~2 minutes before issue occurs, or 10~20 hours before issue occurs?
2. Is it possible to remove the IDC device and have instead…
Part Number: OPA277 Hello, this is Moon.
I am currently using the OPA277 as a buffer. The datasheet provides the output impedance only up to 1 MHz, but I would like to know the output impedance around 200 MHz. My rough estimation is in the range of…
Hi Chris,
1. We do not have the breakdown of NF for LNA and mixer separately.
2. No, the RX Gain range of 18dB means the RX Gain can be programmed from 30dB to 48dB.
3. Yes, the RX conversion gain means the total gain of RX chain. It signifies that…