1. For isolating RF related issues, in this case being the HPF not effecting the point cloud the way we expect it to, it is a good idea to minimize the amount of processing that occurs on the radar data outside of the main FFTs. We make it easier to narrow…
Hi Aden,
thank yo for comment.
I'm checking if i can use a 22uF Tantalum polymer cap, something like T529P226M006AAE150 (22uF 6.3V 150mOhm).
But this one has 150mOhm ESR. Can a single 100nF 0402 ESR help tp lower the total ESR of the tantalum…
The Local Oscillator (LO) is not a fixed 20 GHz signal. Instead, it follows a specific frequency range that depends on your programmed chirp parameters. The AWR2243 generates a internal LO between 19 GHz and 20.25 GHz . This LO signal carries the actual…
Part Number: OPA858
Hi Team,
Posting on behalf of our customer.
I am evaluating a TIA for a CMUT ultrasound application. I am currently considering the OPA858. The application is very similar to a standard photodiode application. I therefore used…
Hello Jordan.
Glad to hear that is helping.
Jordan Schultz said: 1. Can you point me to a doc that explains how SNR is calculated? I am quite familiar with SNR in other branches of signal processing, but wanted to dive a little deeper to understand…
Hi Abhishek,
This frequency range is kind of odd, Analog RF doesn't have anything that goes this low in frequency. Take a look at this forum post on stack exchange for some recommendations for op-amp + switch implementation.
https://electronics.stackexchange…
Hello Torry,
The op-amp is working, but it is acting like a comparator. VIN+ > VIN- = output high (4.6V).
Possibilities:
1. Short somewhere on IN- node (0V? Should also be 2.3V)
2. Bad/open Rf
3. Leaky (reversed) 100uF cap
4. Damaged TLV6741…
You can refer to the .map file of the new program to estimate the flash address range that needs to be copied or programmed. The map file provides the start addresses and sizes of the linked sections, and also lists the memory regions along with their…
Part Number: TPS2HB50-Q1 Other Parts Discussed in Thread: TPS1HTC100-Q1 , TPS1HB50-Q1 Tool/software: Hello, My customer would like to know terminal capacitance of EN pin for TPS2HB50-Q1, TPS1HB50-Q1 and TPS1HTC100-Q1 respectively. They would like to put…
Part Number: IWRL6432AOPEVM Other Parts Discussed in Thread: IWRL6432AOP Tool/software: hi there,
i'd like to estimate range and rcs when playing around with radar configuration. since this is not calculated by the mmwave sensing estimator in the advanced…