Hi Miguel,
Thank you for your reply!
I have one more question, please see here , P8.1 (MSP430) will be connected to BT_HCI_RTS (PAN1315), but on p.19 (the 1st block diagram) of " MSP430BT5190 +CC2560 EtherMind Bluetooth SDK Developer Guide", P1…
-I've proceeded to create 2 partitions, since I have the Bone and not the EVM.
-I installed SD card contents, and
-then created an SD card using the pre-built images from the SDK rather than enter in custom boot and rootfs file path (I hope that step…
Hi Vivek,
Thanks for your post.
The foremost criteria is that, you need to ensure your USB web cam supports composite video/image capture to run face detect demo on omapl138 lcdk. Usually, the input would be captured with the standard Composite camera…
Hi Darin,
Referencing:
Section 2.2 "Digital Frame Sync" in the AWR1243 Cascade Radar Application Note: http://www.ti.com/lit/pdf/swra574
AWR1xxx Data Path Programmers Guide: http://www.ti.com/lit/pdf/swra555
The RX ADC sampling windows are…
i am using a AM335x Starter Kit from Sirtex. output of cpuinfo Processor : ARMv7 Processor rev 2 (v7l) BogoMIPS : 718.02 Features : swp half thumb fastmult vfp edsp thumbee neon vfpv3 tls CPU implementer : 0x41 CPU architecture: 7 CPU variant : 0x3 CPU…
Other Parts Discussed in Thread: SYSBIOS Is there a worked example for DM8168 somewhere showing how to route the
Ducati BIOS debug to the Linux Cortex-A8 host, using the UIA?
The SDK 5.00.00.11 release had some commented-out memory maps
and…
Hello
I would like to find a tool chain for BeagleBoard XM rev C
SDK , UBoot with angstom OS . like to work with Linux Kernel 2.6.32 or 2.6.38
Also I like to format new fresh microSD for that puropse - what is the way not to delete the current…
Hi Renan,
I am using timer example program as base for this binary file creation. The binary file is created at this folder location " C:\ti\CC3200SDK\cc3200-sdk\example\timer\ccs\Release ."
As I have said the binary file is only generated when I…
Part Number: LMX2615-SP Other Parts Discussed in Thread: LMX2624-SP lmx2615-sp_DEC 2025.pdf lmx2615-sp_MAY 2020.pdf
Is the specification of output of lmx2615-sp really changed?
PLL_bufferAMP_output.pptx