Part Number: SM74611 Hello,
I am designing a solar panel array and considering using ideal bypass diodes every 3 solar cells for a high school project.
The array has approximately 150 cells where any number of them could be shaded. The project is a solar…
Part Number: SM74611 Other Parts Discussed in Thread: LM5050-1 Hi there,
We used the SM74611 diode for our voltage regulation application for single board computer. It needs 3.3V and 2 ampers for operation. Single board computer couldn't start because…
Part Number: SM74611 I am doing an application about ultrasound energy transfer.
As output of my ultrasound receiver I have an AC signal of frequency around 70 kHz and amplitude of about 150 mV. The current, flowing through an optimum resistor load,…
Part Number: SM74611 Other Parts Discussed in Thread: TINA-TI I'm trying to import this PSpice transient model into TINA TI using the new macro wizard, but I get the aforementioned error. How can I fix this?
Part Number: SM74611 Other Parts Discussed in Thread: LM74700-Q1 I have 2 12 vdc batteries of similar but unequal type. I want to isolate one from the other during discharge, none should charge or drain the other. Voltage drop must be small - there is…
Part Number: SM74611
Hello E2E,
Q1; I could not import the sim-model file for SM74611 to my PC. Does TI have the new sim-model file?
Q2; I'd like to use this device for energy harvesting. I understood that Vf of this device is 26mV(at 8A) from datasheet…
Part Number: SM74611 Other Parts Discussed in Thread: LM74610-Q1 , LM74700-Q1 I have seven 12V PV panels that are to be connected in parallel to generate the current required for my application.
Each panel has it's own integral 'bypass' diode across the…