Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505A , ISO1042 Hello TI Team,
Please review the attached SN6505A circuit.
Design Contains 3.3V to 5V Isolated circuit and Ioslated CAN Transciever.
Please review both ASAP
Konnect-4G_Outjob.PD…
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505B , SN6505A Hi team,
There are many transformers which TI recommend in the SN6505A-Q1 datasheet. However, there are no transformers that meet the following customer requirements:
1、5V to 5V …
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: THS4081 Manuel
Looking for an SOT-89 pkg LDO that can handle 12-15 V input, give 5.2v output to drive SN6505 which has multiple isolated outputs? The total current from 5.2V running the SN6505 is…
Hi Tiger,
As Clemens pointed out, ISOUSB211DPEVM uses SN6505A for isolated the power and generating 5V output from 5V input. Please refer to Table 9-3 on SN6505A datasheet for the list of suggested transformers from different vendors for various input…
Part Number: SN6505A
Hi team,
My customer will use SN6505A for his application and he is asking some basic questions.
Is it okay to input clock to CLK pin while the device is disabled as long as CLK pin satisfies rating?
As for sequence for each pins…
Part Number: SN6505A Other Parts Discussed in Thread: SN6505B , Hi Sir,
May we know that SN650x series can input +5V and output -5V isolation application?
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505A Hello Team,
Attached is the schematic which uses "SN6505AQDBVTQ1" and "750316032" Transformer for having Isolated power from 3.3V to 5V.
I testing the same circuit with…
Part Number: SN6505A Other Parts Discussed in Thread: SN6505B Hello expert,
May I know if SN6505A or B could support 3.3Vin->5Vout/430mA? Customer would like to use PH9384.012NL(1:2 push pull transformer) and input current might be higher than 1A, right…
Part Number: SN6505A Other Parts Discussed in Thread: SN6505B , SN6501 , Hi Team,
On page 25 on the SN6505 data sheet, reference Table 3, there is reference to a Wurth transformer (750313710) that can be used with the SN6505B driver with a winding ratio…
Part Number: SN6505A Other Parts Discussed in Thread: STRIKE Hi team,
My customer will use SN6505A.
He is doing EMC test on his product and SN6505A seems stop switching when ESD test.
He understands this is not device matter and should optimize his board…