Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505B , SN6501 , SN6505A We are currently using the following MIDCOM component (750343725) for SN6505A-Q1 (transformer driver) ; is there an alternative to the 750343725? Anything from Texas Instruments…
Part Number: SN6505B Other Parts Discussed in Thread: SN6505A , Hi Teams,
We want use SN65055 to design a isolation gate driver power, the specification :
Input: 5V Output: 23V/100mA (18V/-5V 100mA) Isolation: 1500V
But we use Tina simulation SN6505A + 750316856…
Part Number: SN6505A Hello,
On the SN6505A EVM, the transformer provides 5kV of isolation. Do we have a recommendation for 8kV or higher? Preferably 12kV.
Thanks, Nick
Part Number: SN6505A Other Parts Discussed in Thread: SN6505B My customer is surveying one DC/DC isolation. Here is a requirement.
Vin range = 9~15Vdc +
Power IC can output isolation Vout = 12Vdc/0.2~0.5A
Isolation > 1kV
Based on above, we found the…
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505A , SN6505B-Q1 , , SN6505B Hello Anant-san,
Could you give me the SN6505A/B-Q1 comparison data about efficiency vs load current, which is tested by using the same trans. but different frequency…
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505A
Hello,
I would like to use the SN6505A-Q1 device to isolate 5V and generate a 5V and 10V output voltage. Is it possible to use a single transformer solution as shown below? It seems…
Part Number: SN6505A Other Parts Discussed in Thread: SN6505B , , SN6501 SN6505A's efficiency is 3% or lower when temperature is +25 degrees Celsius compared to -40 degrees Celsius and +85 degrees Celsius. SN6505B shows the same features in the same…
Part Number: SN6505A Hi ISO team,
I'm posting this question on behalf of my customer.
Can the input enable pin be driven directly with a GPIO from an MCU (sits at 3.3V)?
Thank you for your response,
Lauren
Part Number: SN6505A Hi team,
My customer considers to use SN6505A and provided some questions.
Is it okay to have unbalanced load when bipolar output configuration like Figure.48? e.g. For Positive supply side: 300mA For Minus supply side: 20mA
Could…