Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505B-Q1 , , SN6505A , SN6505B Hi,
Now, PCB size is small, What is the minimum size of transformer? SN6505A-Q1,SN6505B-Q1,
output current is small ,200mA.
SN6505A-Q1,SN6505B-Q1, differentoperating…
Part Number: SN6505A Other Parts Discussed in Thread: SN6505B When increasing the temperature of driver upto 85'C ,the D1,D2 dead time current drastically increases to 2A-4A AND Output voltages decreases.
During higher temperature the Driver Transformer…
Part Number: SN6501 Other Parts Discussed in Thread: SN6505A , SN6505B Hi TI,
How was this issue resolved?
I am using SN6505a.
I am facing a similar issue, where switching frequency of D1,D2 is reduced to 4kHz when operated at 85'C, it remains unstable…
Part Number: SN6505A Hello,
I would like to know if the internal oscillator has had any testing and certification done to confirm performance?
Specifically, have any safety organisations such as UL, TUV, VDE, etc. confirmed performance and reliability…
Hi Tim,
Thanks for following up with more questions, please see my inputs below.
ISOUSB111 is only a data isolator and power isolation needs to be done separately. Hence, it doesn't generate 5V by itself to the downstream side.
The EVM for ISOUSB111…
Part Number: SN6505A-Q1 Hello team,
Could you tell me Ron value @ TA=125℃? I saw it @ TA=25℃ in datasheet, but I also would like to know it @ TA=125℃.
Best regards, Ochi
Part Number: SN6505A-Q1 Hello team,
It is related question to SN6505B: What is Ron @ TA=125℃? .
Could you tell me the reason why SN6505-Q1 has lower Ron if it is higher temperature?
You said that ' The overall minimum value of R(ON) is going to happen…
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6501 , SN6505A Hi,
We are in the need of an isolated power supply of around 40V capable of supplying around 5 to 10 mA (we need to supply just one IC high voltage power input). We do not need a…
Part Number: SN6505B-Q1 Other Parts Discussed in Thread: SN6505A-Q1 , SN6505B , SN6505A Hi team,
Nice to meet you by email. I am writing to ask the difference between SN6505B-Q1 and SN6505A-Q1. Because from below compare table, I didn't know their difference…
Part Number: SN6505A Hello team,
one of my customers is planning too use the SN6505A with a Vin in the range of 4.5-5V. Sot hey follow in this case
So they will have a non regulated 5V line isolated but they need to obtain from it a 3.3V regulated…