Part Number: SN6505B I want to design a low-noise measurement power supply with a range of +5V to +/-12V (up to +/-15V).
Analog Engineer's Circuit:Precision, +/-15V Power Supply Circuit From a +5V Source for High-Voltage Data Converters. The transformer…
Part Number: SN6505B Hi,
I'm evaluating SN6505B and I have added a load on the secondary side of appr 130mA. The driver SN6505B is patched onto my board but I have tried to keep the patch wires short and tight.
The output from the tranformer is fed…
Part Number: SN6505B Tool/software: Hi Team,
Can SN6505B meet the NBIOT Module conditions?
• VINP = 5.5V:
When the ambient temperature is -40°C, the maximum output current is about 170 mA
When the ambient temperature is 25°C, the maximum output…
Part Number: SN6505B Other Parts Discussed in Thread: SN6501 Need to know if it's possible to monitor current for the SN6505B transformer driver by putting a current sense resistor between Pin 4 and GND. If you do this does it effect the operation of…
Part Number: SN6505B-Q1 Tool/software: Hello,
does the overtemperature event have an impact on the lifetime of the component or is the thermal shutdown protecting the component so that it has no impact?
BR
Simon
Part Number: SN6505B Tool/software: Hello experts,
I prepare to use SN6505 to design a push-pull circuit. The transform we used is Bourns HCTSM80308BAL, Turns Ratio 3:8.
I have some questions shown as below:
1、How to calculate the push-pull circuit…
Part Number: SN6505B-Q1 Other Parts Discussed in Thread: SN6505B Hii
We have a requiremnt of desiging isolated power supply . Following are the specification:
Vin :5V
Vout:12V
Iout : 350mA(max)
for desging we have selected the SN6505B push pull…
Part Number: SN6505B-Q1 Other Parts Discussed in Thread: SN6505B Hi team,
Does SN6505B-Q1 support design with VIN=5V and VOUT=3.3V? If so, could you provide design solutions?
BR,
Jade Lan
Part Number: SN6505B-Q1 Other Parts Discussed in Thread: SN6507 Tool/software: We are testing the SN6505B-Q1 in a half-wave rectifier configuration with the Wurth 760390014. We are observing an issue where the push-pull stage stops switching. What I want…
Part Number: SN6505B Other Parts Discussed in Thread: SN6507
Tool/software:
Hello,
I need an isolated 24VDC power supply (50mA minimum) that is generated from the 5VDC.
Can I use a SN6505B with a transformer flipped 180°: 750319694 or 750317828…