Part Number: SN6505B-Q1 Hi there,
In the component datasheet, all reference design are using same voltage for SN6505B-Q1 (VCC) and primary winding of transformer.
In my application i would like to have two different voltages, for:
…
Part Number: SN6505B This circuit generates a negative isolated 15V
At higher air temperatures >= 65°C the output skips operation - load is around 55mA average
What could be the issue here?
Part Number: SN6505B Other Parts Discussed in Thread: TPS7A05 , SN6505A Hi,
We have to power supply a 4 channels isolated data acquisition system and we are looking for an ultra low-power isolated DC-DC converter with the following specs:
VIN: from a 3…
Part Number: SN6505B-Q1 Other Parts Discussed in Thread: SN6501-Q1 , SN6505A-Q1 Hi, can you advice me with a better part for EMC performance than SN6505B-Q1? Today I'm using this part for the push-pull converter of insulated gate driver power supply, but…
Hello Vamsi,
I apologize for the confusion. I meant to show that I have provided the information to your questions regarding gate charge and rise and fall time in my initial reply, please review and follow up with additional questions or information here…
Part Number: SN6505B Other Parts Discussed in Thread: SN6501 , , SN6507 Hi team,
Recently my customer is evaluating SN6501 and SN6505B, some questions about protection and safety came up. Could you pls help with these questions? Thanks a lot!
SN6505B:
…
Part Number: SN6505B-Q1 I want to confirm if it is ok that I design for output higher than 30V, like 31V?
If not ok , what limits the output, the internal MOSFET?
Part Number: SN6505B
Customer has built product giving the SN6505 5V supply, whilst providing the enable pin 3.3V.
Customer is trying to determine how much exposure they have with this setup.
What is the typical multiplier for the enable? (0.55x?)
What…