Part Number: SN6507-Q1 Other Parts Discussed in Thread: SN6507 Hi Team,
I would like to check with you if there have calculation tools for SN6507-Q1 to better support customer's design? Like the transformer parameter calculation tool?
If yes, please…
Part Number: SN6507-Q1 Other Parts Discussed in Thread: SN6501-Q1 , SN6501 , SN6507 Hi,
Good Day.
Is it possible to use the component SN6507-Q1 as equivalent to the not available SN6501-Q1 in order to drive a transformer 1:1 at 12V for an isolated supply…
Part Number: SN6507-Q1 Other Parts Discussed in Thread: SN6507 Hi team
We notice that SN6507 has spread spectrum function, what's the frequency range? Like for 1MHz, what's the percentage for SSC? 5%?
Part Number: SN6507 Other Parts Discussed in Thread: UCC25800-Q1 Dear Specialists,
My customer is interested in SN6507 and has a question.
I would be grateful if you could advise.
---
I would like to design a 12V, 24V, 48V isolated power supply circuit…
Part Number: SN6505A Other Parts Discussed in Thread: UCC25800 , UCC25800-Q1 , SN6507 Hi, we are using the Würth 750315240 transformers in series to build a high voltage isolator.
It works really well with the LT3439, but now we want to try the 6505A…
Part Number: UCC14131-Q1 Other Parts Discussed in Thread: UCC25800-Q1 , UCC14240-Q1 , SN6501-Q1 , LM5180-Q1 , SN6507 , UCC25800
Hi Expert Iam working on topology trade off between different isolated gate driver bias supply for cascoded GaN. I have performing…
Hi David,
Please consider first that Q5, C4, D4, R2 and Q4 are not used, therefore C3, R1 and Q3 are connected directly to J1 (24Vin) by means of R100 and R3, which are both 0 Ohm resistors. Vdd of the SN6501 is supplied by Q3, while Vcc is kept to D3…
Other Parts Discussed in Thread: UCC12041-Q1 , SN6507 Hi Team,
I am looking for Isolated power supply to drive the high side SiC MOSFET 1700V. With Below specification
Input Voltage=5V
Output Voltage=15V
Isolation Level=3KV or more
AEC-Q100 or AEC-Q101…
Part Number: SN6505D-Q1 Other Parts Discussed in Thread: SN6505B , SN6501 , SN6507
Hello there,
Is the SN6505B/D still recommended for new designs? We have been trying to order it for more than a year and a half without success. Is there any (ideally pin…