Part Number: SN65HVD101 Other Parts Discussed in Thread: SN65HVD102 , Hello Team,
the customer would like to replace the SN65HVD102 with the SN65HVD101 due to better internal availability.
The LDO output would remain floating.
Is this a problem?
Considering…
Part Number: SN65HVD102 Other Parts Discussed in Thread: TIOL111 Hello Folks,
We have some sensors that can communicate over IO-Link.
And we need to communicate with these sensors via IO-Link, so my Linux Machine will be the IO-Link master.
So here I…
Part Number: SN65HVD102 Other Parts Discussed in Thread: MSP-EXP430FR4133 , SN65HVD101 Hi team,
our customer is using SN65HVD102 for IO-Link PHY and plan test IO-Link certification. feedback from customer that they need provide TI reference design to …
Part Number: SN65HVD102
Hello Team,
I have a board where the nc pins 2,9,11 are connected to ground, while they should remain not connected.
The PCB is currently done. Would the ground connection affect the performance or damage the part?
Are those pins…
Part Number: SN65HVD102 Hello Team,
the SN65HVD10x has a driver enable delay that is specified by max. 5us.
We do see that the majority of the device actually have a delay more in the range of 1us but there are very few that are in the range of 3us. …
Other Parts Discussed in Thread: SN65HVD102 , SN65HVD101 , SN65HVD101EVM Hello.
Please tell it about failsafe function of SN65HVD102.
My customer checked on an action in CQ voltage = OPEN of SN65HVD102. Then the High output became Low after that in around…
Other Parts Discussed in Thread: SN65HVD102 Hi,
I am new to io link protocol and need help in developing pressure sensor with io link interface using SN65HVD102. I have some questions regarding this,
How to specify requirement for io link? How to create…
Other Parts Discussed in Thread: SN65HVD102 Hello,
I connected the SN65HVD102 with my MCU.
And the MCU has a UART-bootloader with same RX and TX lines from SN65HVD102.
Now i want to connect these TX, RX lines with a FT232RL von FTDI and use the bootlo…
Part Number: TIOL1123 Other Parts Discussed in Thread: SN65HVD101 , , TIOL112 , TIOL111 , SN65HVD102 Hi, we use SN65HVD101 IO-Link PHY for our IO-Link devices. We consider switch to TIOL1123. There are some differences between these transceivers and differences…
Hi Athul,
I'll move this post to the High Speed Amplifiers forum, since they should be able to give better guidance with regard to LM7171. In addition, you may want to take a look at the SN65HVD101 and SN65HVD102 devices. These can support the voltage…