Hi Patrick,
The CAN2.0 specification actually doesn't include the physical layer characteristics that would be relevant for a transceiver chip like SN65HVD1040. It relates more to the CAN protocol/data link layer. The physical layer (i.e., properties…
Other Parts Discussed in Thread: SN65HVD1040 We got the request of P-Spice model for SN65HVDA1040-Q1.
I think there is not it (I confirmed "SN65HVD1040", but there is not it too.).
If we request it, can you provide it? And if possible, when will we…
Other Parts Discussed in Thread: SN65HVD257 , SN65HVD1040 , SN65HVD255 , SN65HVDA1040A , SN65HVD256 Hello, all
Now we are considering to use SN65HVD257, then would like to know the detail on the maximum signaling rates on this device.
When referring…
Other Parts Discussed in Thread: SN65HVD1040 I am sharing a connector with RS485/422/CAN in the design, and I am trying to make them bias correctly.
In CAN bus, SN65HVD1040 datasheet mentioned a solution with split termination network.
But TI AN847…
Hi Linda,
You will always be limited by the total propagation delay in a system. I good rule of thumb is to keep the delay of isolator, transceiver and cabling in both directions to less than 1/2 the bit time. What do you mean by "the original ISO7221B…
Hi José,
José Arbugeri said: Firstly, I encountered an issue with this topology where one port of node loses connection with the network, causing the transceiver to become unterminated (60R). This situation leads to an unattenuated signal, and the transition…
Ram,
Here are the following bxls that the vendor was able to generate:
1. 4544.INA333-HT_HKQ_8.bxl
2. 4527.SM28VLT32-HT_HKN_14.bxl
3. 0383.REF5025-HT_HKQ_8.bxl
4. 7041.ADS8320-HT_HKQ_8.bxl
5. 7457.SN65HVD11-HT_HKQ_8.bxl
The above 5 bxls…
Part Number: LP-AM263 Other Parts Discussed in Thread: TCAN1043A-Q1 Hello, does there is a code which can support this CAN transceiver ?
www.nxp.com/.../TJA1463.pdf