Part Number: SN65LVDS1 Other Parts Discussed in Thread: DS90CR287 , About SN65LVDS1 and DS90CR287, Is there tolerance spec for Overshoot and Undershoot?
(For example; V/ns etc)
Best regards,
Satoshi
Part Number: SN65LVDS1
Hi , can two SN65LVDS1 drivers a single SN65LVDST2 receiver.
The line length is 3', a DS1 and DST2 resides at each end. The 2nd DS1 is a foot from the first.
Is this a possible, schematically what would the BUS look like?
…
Part Number: SN65LVDS1 Hello Team,
Could you please advise us if SN65LVDS1 could be used with AC coupled connection ?
I worried about the DC path when used at AC coupled. If the device requires external resistors, could you please provide us your recommended…
Part Number: SN65LVDS1 Other Parts Discussed in Thread: SN65LVDS2 ,
Dear Technical Support Team,
I have two questions for SN65LVDS1 and SN65LVDS2.
1.)Could you tell me "Differential Part to Part Skew" ?
2.)Could you tell me the min value of Propagation…
Part Number: TPS7A45 Other Parts Discussed in Thread: SN65LVDS2 , SN65LVDS1
We are using a cascaded configuration of TPS7A4501 to supply 2x SN65LVDS1 and 2x SN65LVDS2 so around 30mA max.
As we are powering the circuit in sequence and we can't soft start…
Part Number: SN65LVDS4 Other Parts Discussed in Thread: DS90LV017A , SN65LVDS1 , DS10BR150 Do you make a 500mhz LVCMOS to LVDS translator or buffer or converter?
All the ones I've found seem to top out at around 250Mhz or so.
Thanks,
Part Number: SN65LVDS4 Other Parts Discussed in Thread: SN65LVDS1 Hi I was looking at the SN65LVDS4 which looks like a pretty cool 1.8V part. On the data sheet in typical application circuits it shows a single ended to differential driver providing the…
Other Parts Discussed in Thread: CDCV304 , SN65LVDS1 Hi Team,
Our customer is considering to use CDCV304 and SN65LVDS1 as they have these device registered in their company.
[Question] Can you drive two SN65LVDS1 from one of the CDCV304 output channel ? …
Other Parts Discussed in Thread: SN65LVDS1 , SN65LVDT2 Recently a customer returned a unit where 2 SN65LVDS1 were no longer driving signals. Outputs Z and Y were both at ground level. Is this failure due to a voltage or current overload? Measuring resistance…
Part Number: DS90LV017A Other Parts Discussed in Thread: SN65LVDS1 , DS90LV011A
Hello,
Could you help find a proper device for customer requirement below? I thought DS90LV017A or SN65LVDS1 might fit but it supports only 3.3V. Please let me know if we…