Part Number: SN65LVDS104 Other Parts Discussed in Thread: SN65LVDS22 , TMUX1309 Tool/software: I'm looking for an LVDS clock multiplexer. Essentially the opposite of the SN65LVDS104 repeater, i.e. 4:1 LVDS. Any suggestions? Thanks
Part Number: SN65LVDS104 Hi,
Could you please let us know the Tj range under recommended operating conditions on SN65LVDS104?
Please advise us.
Thanks and best regards, M.HATTORI.
Harish
SN65LVDS104 is not the right solution for designing a HDMI splitter. Unfortunately we do not have a HDMI splitter solution in our product portfolio.
Thanks
David
Part Number: SN65LVDS104 Hello Team,
customer has a question about lvds buffering.
"We need to be able to drive four 100Ohm terminated receivers in a multidrop configuration. The termination is internal so not removable thus leads to a 25ohm termination…
Part Number: SN65LVDS104 When using the ibis model to simulate the SN65LVDS104 part in our system using HyperLynx, when simulating at fast-strong the output differential CM drops from 1.2V (what we see with slow-weak or nominal) to around 0.82V and the…
Part Number: SN65LVDS104 Other Parts Discussed in Thread: CDCLVD1213 , LMK00334 Hi All,
I was considering using the SN65LVDS104 for an LVDS clock distribution application. Do you have any parts similar to this, or any other LVDS repeaters or CLK distribution…
Part Number: SN65LVDS104 Hello,
Although it is obviously not best practice, do you see any major problem with having an idle/non-changing input (IN+ stays high, while IN- stays low) while the chip is in an un-powered state? This situation might be un…
Part Number: SN65LVDS104 Hi,all
The SN65LVDS104,unused LVDS output pairs can be floating(ENx=Low)?
and if ENx=High,unused output pairs floating,will introducing switching noise?Thanks。
regards,
guo