Part Number: SN65LVDS9637 Tool/software: Dear TI Support Team,
I hope this message finds you well.
I am reaching out regarding an issue I have encountered with the SN65LVDS9637 differential to LVDS receiver in one of my designs. To provide some…
Part Number: SN65LVDS9637 Hi, I'm trying to get an idea of how the SN65LVDS9637 output would interface with an i2c bus. In particular, I want to know if it can handle the acknowledge bit from an i2c slave device. The SN65LVDS9637 has an output fail safe…
Part Number: SN65LVDS9637 Hello!
We're utilizing TI's LVDS receivers in one of our designs in a high noise environment. The receiver has the following table:
Is the output between the +/- 100mV threshold indeterminate because it's not time invariant…
Part Number: SN65LVDS9637 Hello support team,
My customer would like to know typical value of the Vit+ and Vit- for SN65LVDS9637 since the datasheet mentioned it as only Max and Min.
Would it be possible to provide that value?
Best regards,
…
Part Number: SN55LVDS32 Other Parts Discussed in Thread: SN65LVDS9637 , SN65LVDS3486 , SN65LVDS32 , Tool/software: What is the thermal rise for the FK package? The datasheet shows thermal rise information for the SN65LVDS32, SN65LVDS9637 and SN65LVDS3486…
Other Parts Discussed in Thread: SN65LVDS9637 I am looking for a LVDS Line Receiver with Ultra-Low Pulse Skew with a fail-safe circuit - when one of the inputs is open, the output should be HIGH. Of course, it should also give HIGH output for other failures…
Hi Tobyn,
Attached is the IBIS model for the SN65LVDS9637. Please let me know if this issue persists.
8203.sllc018.ibs
Regards,
Michael Peffers
High Speed Interface Applications
Other Parts Discussed in Thread: SN65LVDS9637 , ADS5485 , ADS5400 I want to interface a high speed ADC such as the ADS5485 with a relatively low power DSP with sleep modes. The high speed ADCs tend to use LVDS outputs and DDR. A differential line receiver…
Part Number: LM98620
Hi Team,
CIS output is DC signal and the output range is about 800mV.
Now we use SH2b working mode. We refer to the 0638.LM98620_register_example_Dec2020.pdf that reg 01 with value 48, reg 23 with value 00.
The schematic…