Part Number: SN65LVELT23 Hello,
The output pin is connected to GPIO of MCU and is interrupt source. The input pins are connected to external connector without any termination resistors, and external connector is opened.
I attached a picture, ch3/ch4…
Other Parts Discussed in Thread: SN65LVELT23 Dear Sir/Madam,
There are queries which need inputs from the company for the following part: SN65LVELT23
1) What is the process technology used to fabricate the SN65LVELT23, is it purely based on bipolar…
Other Parts Discussed in Thread: SN65LVELT23 Hello,
SN65LVELT23 incorporates a input pull-up and pull-down resistor.
Is thevenin termination resistor necessary for input of LVPECL(SN65LVELT23)?
Best regards, Seishin
Hi there, any chance that the datasheet will be updated with clear LVDS input specification soon? This answer is from 2013 and datasheet still from 2009.
thanks
David
Other Parts Discussed in Thread: SN65LVELT23 Hello,
I am dealing with a design that may encounter open LVPECL inputs on SN65LVELT23 (LVPECL to LVTTL translator). From the data sheet, I can see the device has two 50k pull resistors guaranteeing 'Vcc…
Part Number: LMK1C1102 Other Parts Discussed in Thread: TLV3801-Q1 , SN65LVELT23 , LM27762 , CD74HC4053 , TMUX4053 , TMUX1072 , TMUX1574 , , TLV3801 Tool/software: My goal is to take two types of signal into a device
single ended +/- 1 V sine wave…
Part Number: LMK1C1104 Other Parts Discussed in Thread: LMK01000 , LMK04832 , SN65LVELT23 , LMX2820 , LMX2594 , DDS39RF10 Tool/software: Hi,
I would like to generate single ended CMOS clocks (< 250 MHz) with 10%, 25%, 50% and 75% duty cycle on the board…
Part Number: LMH1983 Other Parts Discussed in Thread: SN65LVELT23 Hi Experts, My customer would like to convert to LVTTL for LMH1983 output. Customer would like to use SN65LVELT23, then customer has question. 1. It can connect directly between LMH1983…
Part Number: SN65LVELT22 Other Parts Discussed in Thread: SN65LVELT23 1. My design is TTL to LVPECL signal driving optical module, with sn65lvelt22 / sn65lvelt23;
2、帮忙核查LVPECL部分交流偶合到光模块部分原理图是否正确;
2. Help to check whether the schematic diagram of LVPECL…