Part Number: SN74LVC07A Other Parts Discussed in Thread: SN7417 , SN7407 , TPIC6C595 , TPL7407LA Hi, Support Team
Do we have Similar with SN74LVC07A, but we need open drain output 12v
Typical Vcc is 3.3v
if any suggestion, Please advise me.
Thanks,
Best regards…
Other Parts Discussed in Thread: SN7407 Hi,
I am using the output of a SN7407 to drive a TTL input. Do I need a pull-up resistor for the the output?
Thanks.
Other Parts Discussed in Thread: SN74LVC8T245 , SN7407 , SN7404 Hi,
Could you let us know what is the max power consumption for the following devices: SN7407 and SN74LVC8T245, please?
Thanks.
There is the old TTL SN7407. The SN74ALS1035 and SN74ALS35A have lower output currents. If the input signals are not TTL but actually 5 V, the SN74LVC07A might work.
Hi,
I can recommend using the SN7407 open collector device. http://www.ti.com/product/SN7407
It is a buffer which is open collector and allows you to place a pullup resistor on the output to 10V. You will still need a 5V supply to power the device. However…
Part Number: TL084 Other Parts Discussed in Thread: SN7407 Dear sir, I am using a circuit which contains Sn7407 followed by pull-up resistor of 1Kohm and the output on SN7407 is going to the input of TL084.TL084 is used as a voltage follower for switching…
Unfortunately there is not device with higher rating.
The design is the same between the SN7407 and SN5407, just different package, testing, and qualification screening.
If you operate the SN5407 within the SN7407 temperature range, then 40ma will be…
Other Parts Discussed in Thread: SN74LVC2G07 , SN7407 Hello everyone, I believe that my component is related first, is teh SN7407 the generic part number for the SN74LVC2G07?
If not, then according to the datasheet, when I apply a logic high signal to…
Hi Dan ,
This SN7407 I see is open-collector buffers/drivers ,has Y= A Boolean function but since they open collector , you need to pull it high using pull up resistors to Vcc when input is high .