Part Number: SN74AHC1G00-Q1 Hi Team,
Currently my customer is using SN74AHC1G00-Q1 in their design and they didn't found AEC-Q100 qualified in Auto application in our datasheet. So they wondering whether our device can pass AEC-Q100 standard. Could…
Part Number: SN74AHC1G00 Other Parts Discussed in Thread: SN74LVC1G58 , TINA-TI Hi team,
Please check my circuit. If it is normal, there should be an oscillation at R25.
but ...
Please help to analyze it.
Best regards,
Part Number: SN74AHC1G00-Q1 Hello Folks,
I have one question about logic gate (AND)
I have seen that in the datasheet is written: "Schmitt Trigger Action at All Inputs Makes the Circuit Tolerant for Slower Input Rise and Fall Time"
But when i…
Part Number: SN74AHC1G00 Hi
I'm using the 2 input NAND of SN74AHC1G00 with 3.3V of Vcc.
The input A is powered by a pull-up resistor to 3.3V while the input B is connected directly to 3.3V.
What I want to know is that if Vcc slowly drops from 3…
Part Number: SN74AHC1G00-Q1 Hi TI-team
My customer will use SN74AHC1G00-Q1.
They want to know variation of VIH and VIL.
VIH has no description of MAX and VIL has no description of MIN.
Please tell me each.
Best Regards,
Koji Hayashi
Part Number: SN74AHC1G00 Other Parts Discussed in Thread: SN74AHCT1G00 , SN74LVC2T45 Hi,
the power consumption of the SN74AHCT1G00 is specified with a current consumption ICC of max. 10uA (see page 4). There is in the application a high impedance (appr…
Other Parts Discussed in Thread: SN74AHC1G00 , SN74AHC132 , SN74LVC1G98 Hello!
On SN74AHC1G00 product page http://www.ti.com/product/SN74AHC1G00/description
specified, that
" Features ....... Schmitt Trigger Action at All Inputs Makes the Circuit…
Part Number: LM393LV-Q1 Other Parts Discussed in Thread: LM393LV , SN74AHC1G00 Tool/software: Hi,
I've been having a problem lately with comparator of LM393LV.
When the pull-up resistance is too high, port voltage of the comparator is abnormal, port…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: SN74AHC1G00 , SN74AHC1G04 Dear,
I received an error infor shown as below.
ERROR(ORPSIM-16583): Detected an imported model containing transistors or diodes. For such models, PSpice for TI…