Part Number: SN74AHC1G09 Dear Sir / Madam,
In datasheet of SN74AHC1G09DBVR, VOL (max.) has been mentioned as 0.44V under the test condition of, IOL = 4mA, TA = –40°C to +85°C @ VCC = 3V. In our circuit we are using it at IOL = 2.27mA and i want to know…
The output type is shown on the product page:
And the datasheet specifies V OH /I OH , which would not be possible for an open-drain output.
If you need open-drain outputs, then use the SN74AHC1G09-Q1, or add an open-drain buffers (SN74LVC1G07-Q1) after…
Part Number: SN74AHC1G09 Hi team,
Can you please review the following questions for SAN74AHC1G09?
1. For the definition of Vcc+0.7V (please refer to below tables)
-. At Vcc=7V, what is the max. Vo? Is it 7.7V or 7V?
-. At Vcc=3.3V, the max. Vo=4V, so…
Part Number: SN74LVC245A Other Parts Discussed in Thread: SN74HCS21 , , SN74AHC1G09 , SN74HCS11 Hi team,
I would like to know the FIT of the SN29500 standard for SN74LVC245A,SN74HCS21,SN74HCS11,SN74AHC1G09.
Sincerely. Ryu
Other Parts Discussed in Thread: SN74AHC1G09 When Pin 5 (Vcc) of SN74AHC1G09 is low (or connected to ground), what happens when an external high is put on the inputs or the output?
Regards, Anthony
Part Number: OMAP-L138 Other Parts Discussed in Thread: SN74AHC1G09 ,
I use 96MBytes Nor Flash by CS2,CS3,CS5.
Is "the hardware connect" below OK?
Thank you very much!
Hi Andrei,
i made some modification but still couldnt get it to work without interrupt but with external AND.
To make sure the 2 timers are synchron, i use the TIMER_A1_BASE(4MHz) as "burst rectangle" generator and wire this externally as input clock for…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…