Other Parts Discussed in Thread: SN74AUC245 Hi,
I'm looking for a level translator that can convert an RGMII interface running at 125MHz from 3.3V to 1.5/1.8V in HSTL single ended forms.
Does SN74AUC245 have operating experience in RGMII interface ?…
Part Number: SN74LVC1G14-Q1 Other Parts Discussed in Thread: SN74AUC245 , SN74AUC244 Hi Experts,
I'm looking for some single bit buffer that could support tpd less than 1ns. Not sure if any standard logic component could support this. or any thing else…
Hi Abhishek,
The LV family is really optimized for 3.3V to 5V operation.
If you're wanted to do 1.5V to 2.2V operation, I would recommend going with something more modern like the SN74AUC245 -- it's optimized for 1.8V operation, so you will see much better…
Hi Vignesh,
What is the output drive current? If you are driving a purely capacitive load, then the output voltage of any CMOS device will be ~Vdd and GND. if you are driving a heavy resistive load, the VOH/VOL will suffer significantly. I would recommend…
Part Number: SN74AUC16245 Other Parts Discussed in Thread: SN74AUC245 , Logic Team,
I am trying to get the IBIS models for the SN74AUC245 and SN74AUC16245 for a customer. If I go to the product folders, click the "Tools and Software" tab, and…
Other Parts Discussed in Thread: SN74AUC245 Dear Team,
Could you help to recommend the signal buffer solution which is based on the below requirement?
1. 8 bit.
2. Bi-directional
3. For 5V tolerant LVTTL signal.
4. Data rate up to 1 Gbps.
5. The buffer…
Hello JH,
While the SN74AUC245 does not have a rated frequency, the AUC family was designed for >200MHz operation.
This should be a suitable device for this application.
Specifically, the orderable you would be looking for is SN74AUC245ZQNR.
Best…
Other Parts Discussed in Thread: SN74AUC245 , SN74AVC8T245 , LSF0204 , LSF0101 , SN74LV1T34 , TXV0108-Q1 , TXV0106-Q1 I'm looking for a level translator that can convert an RGMII interface running at 125MHz to/from 1.8 and 2.5V.
One candidate I see is SN74AUC245…