Part Number: SN74LVC1G07 Other Parts Discussed in Thread: TXU0104 , SN74AUP1G08 , TXB0104 , TMP1075 , SN74LV244A Hi
As per the standard power dissipation calculation using the Tj and Rtja, the values are more than the power consumption itself. In this case…
Other Parts Discussed in Thread: SN74AUP1G08 Hi,
I've just got the newly revised data sheet of the SN74AUP1G08 LittleLogic Single AND Gate, and all packages apart from the YFP are missing the B input. I'm sure everybody here will agree that a AND gate…
Part Number: SN74AUP1G14 Other Parts Discussed in Thread: SN74AUP1G08 , SN74AUP1G34 Dear Support team,
Logic devices SN74AUP1G14, SN74AUP1G34 and SN74AUP1G08 datasheets specifies the Operating free-air temperature range (TA) from -40 to 85°C whereas Tjmax…
Other Parts Discussed in Thread: SN74AUP1G08 , SN74LVC1G08 Does TI make any 2-input logic AND gate with nA range quiescent current (ultra low leakage) for battery application?
Hi, I am trying this implementation out, and when I turn off VCC_3V3 I am noticing the output goes low for a brief moment before being pulled high (despite the pull-up on the output). Any ideas why that would happen?
For additional information, the L_Z_L…
Part Number: SN74AUP1T14 Other Parts Discussed in Thread: SN74AUP1G08 , Hi Team,
There is a point confusing me. In figue.2 input and output waveform is the same polarity.
But I see the datasheet, Y=A(bar). Is there anything I misunderstand?
Roy
I found SN74HC4060 binary counter and its Icc = 80uA @ 6V. I will need the circuit to work from 3.7V. So I suppose supply current will still be way higher than when using nano timers.
Another option is to use SN74LV163A binary counter and SN74AUP1G08…
Part Number: SN74AUP2G08 Other Parts Discussed in Thread: SN74AUP1G08 Hi,
Is there an IBIS model for the SN74AUP2G08? It doesn't appear under the tools/support tab on the product page.
I can see there is one for SN74AUP1G08, but as this only has one…
Part Number: TPS65910 Other Parts Discussed in Thread: AM3358 , , SN74AUP1G08 Dear Sir,
We use AM3358 + TPS65910A3A+coin-cell backup BAT(220mA 3.2V) for our board.
when main power is off, We use VRTC only mode of TPS65910A3A that backup BAT current is…
Part Number: SN74AUP2G32 Other Parts Discussed in Thread: TINA-TI , , SN74AUP1G08 Tool/software: TINA-TI or Spice Models Hello guys, can you generate an spice/ibis model for this part, or point me to a similar part with equivalent characteristics