Part Number: SN74AVC1T45-Q1 Hi Team
my customer side want to use CAVC1T45QDRYRQ1 SON package.
but we find the package information is missing in datasheet.
www.ti.com/.../sn74avc1t45-q1.pdf
Could you help me provide it?
BRs
…
Part Number: SN74AVC1T45-Q1 Other Parts Discussed in Thread: SN74AXC4T245-Q1 Tool/software: I want to use SN74AVC1T45-Q1 for level-shifting 1.2v Quad-SPI signals to 1.8v. The SPI bus includes standard SPI signals (Clock, Chip Select, Data0-3) plus a dedicated…
Part Number: SN65LVDS4 Other Parts Discussed in Thread: SN74AUC1G125 , DS90LVRA2 , SN74AVC1T45-Q1 Tool/software: I need to translate 200 MHz LVDS clock and associated DDR data to single ended 1.2 V CMOS signals for input to a 1.2 V FPGA bank. SN65LVDS4…
Hi Mythili,
The TXS0101-Q1 will not be able to buffer your signals as its DC drive strength is limited. Consider fixed direction translators, such as TXU0101, 2N7001T, or SN74AVC1T45 instead.
Regards,
Jack
Hello Renan,
Let me talk to our marketing team on how we can bring the datasheet back. For the time being, please see AVC1T datasheet: sces530i.pdf
Regards,
Josh
Other Parts Discussed in Thread: SN74AVC1T45 Hi team,
I understand SN74AVC1T45 supports partial-power-down application using Ioff circuitry, when either VCCA or VCCB is at GND level. Also in the datasheet, it is recommended to power up VCCA followed…
Part Number: TXB0108 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 , TXU0202
We are planning to use level translator TXB0108RUK to traslate the logic level of below signals :;
Digital Outputs coming from IO Expander TXE8124RHBR at…
Dear SIR:
Thank for your reply,But I more confused.Would you base on below question reply directly ?
your reply(A):
I believe condition 4 is what you're looking for.
If B ---> A, then option 4.
If A ---> B, then option 2
your reply (B):
…
Part Number: DP83867IR Other Parts Discussed in Thread: AM3352 Hi expert.
I am drawing a schematic with dp83867
Could you check if the Schematic has something?
I'm gonna use a am3352 processor and connect with RGMII interface.
I attached schematic…