Hi Hans,
I would recommend using one of the SN74AVC series of translators, such as the SN74AVC32T245, which is a 32 bit direction controlled translator capable of 380 Mbps data throughput (which should handle your 165 MHz clock).
Other Parts Discussed in Thread: SN74AVC32T245 What is the channel-to-channel propagation delay skew of the SN74AVC32T245ZKER?
Using operating conditions:
VCCA 3.3V
VCCB 2.5V
Data rate 125Mbps
Thanks Biser,
I got the answer . Just need one more clarifcation
We have two different types of TFT LCD Display , One is 24bit, 4.3 Inch and another one is 18bit , 7 Inch. As per need One LCD can be used at a time.(Two Different Connector on PCB)
Is it …
I see. Well, maybe the TFP401A along with the SN74AVC32T245 will accomplish what you need. The TFP401A accepts TMDS data from 25-165MHz, and deserializes it to parallel RGB 3.3V CMOS. It sounds like your Xilinx requires 1.8V CMOS inputs, so using the …
Other Parts Discussed in Thread: SN74AVC32T245 , TXS0102 , SN74AVCA164245 , SN74LVC1G125 Hi,
How could we determine the output impedance values of logic translators SN74AVCA164245, SN74AVC32T245 and TXS0102?
Thanks.
Mhark
Hello,
I have a question regarding the EVM AM335X LCD schematics. Assuming you loose the VDD_LCD power on U4 (SN74AVC32T245). Since the OE and DIR pins are controlled by the VCCA which is the VDD_LCD how do you ensure the data is not travelled to the…
Other Parts Discussed in Thread: SN75LVDS83B , DS90C3201 , SN74AVC32T245
Since the National acquisition is finalized, I assume that it is OK to ask about this part in these forums now. I need a LVDS transmitter to go from an OMAP (OMAP4430/60) to a dual…
Other Parts Discussed in Thread: SN74AVC32T245 I am using beagle board of revison c3 and I have to inter face that with an LCD.
Beagleboard gives lcd signals (RGB, HSync, VSync etc)of 1.8v and lcd requires signals of 3.3 v .
What parameters should I take…
Other Parts Discussed in Thread: SN74AVC32T245 I am using beagle board of revison c3 and I have to inter face that with an LCD.
Beagleboard gives lcd signals (RGB, HSync, VSync etc)of 1.8v and lcd requires signals of 3.3 v .
What parameters should I take…
Hi Jonathan,
I'm trying to get these pushed to TI.com but I have attached them here for your use.
Regards, Bill
Daughtercard BOM
am335x_gpevm_gpdboard_3H0001_bom_rev1_2b.xlsx
LCD card BOM
am335x_gpevm_lcdaboard_3H0005_bom_rev1_3a.xlsx