Hi,
I need to translate level (3.3V to 2.5V) for signal running up to 150MHz.
I see on TI web site that the SN74AVCB164245 device has 400MSPS max data rate but when I read the datasheet, I don't find this information, why ??
In addition, I need to kn…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: SN74LVCR16245A , SN74AVCB164245 We're looking for an alternative to SN74LVC16T245, that integrates either the ~25ohm damping Res or DOC (Dynamic Output Control) circuitry. Also needs to be 5V…
Hi Alice,
Would the customer consider using the non-bushold version of the same device SN74AVCB164245?
These do not have bus hold circuitry internally and hence can have external pull up resistors.
For more information on bus hold devices and design…
Markus ,
what is the translation voltage requirements ?
I can suggest you to use either the -Q1 automotive grade part www.ti.com/.../sn74avcb164245-q1.pdf
or www.ti.com/.../sn74avc16t245-q1
or sn74lvc16t245-EP device qualified for military from -55…
Other Parts Discussed in Thread: SN74AVCB164245 Hi,
In the Description/Ordering Information section of the SN74AVCB324245 's datasheet it is specified that "The SN74AVCB324245 is designed so that the control pins (1DIR, 2DIR, 1OE and 2OE) are supplied…
Hi All,
I simply need to know how to calculate the Bandwidth of the following product: http://www.ti.com/lit/ds/symlink/ sn74avcb164245-ep .pdf
What I need is not just an answer. I need to learn the method. There is no info about, rise time, bandwidth etc…
Thank you for your reply,
Generalisations about families are okay, but >100Mbps or <25 is not sufficient. How much big or small? Moreover, there are TXB-family products claiming >100Mbps data rate for instance. Generalisations may fail. Tthere are other…
Hi,
You can use the SN74AVCB164245 , it doesn't have series resistor but it has output impedance dinamic control (DOC). You can read about DOC here:
http://www.ti.com/lit/an/scea009b/scea009b.pdf
If you need bus hold, there is also a SN74AVCBH164245…
Other Parts Discussed in Thread: TVP5146 , SN74AVCB164245
Has anyone used the daughter card connector D4 on a Da Vinci 6446 EVM to do Master Mode Video capture. Please detail what you
did to get this working . . .
Thanks TPC1