Part Number: SN74CB3T1G125 Other Parts Discussed in Thread: TS5A4594
Do we have a device like the SN74CB3T1G125 with an enable that is active high?
Jay
Other Parts Discussed in Thread: SN74CB3T1G125 Hello,
I’ve got a 300kHz clock problem with SN74CB3T1G125. The input signal looks pretty good, the output signal has a “high problem”, please see the attached scope shots.
I’ve also attached the schematic…
Other Parts Discussed in Thread: SN74CB3T1G125 , SN74LVC1T45 Hi all Would you mind if we ask SN74LVC1T45 and SN74CB3T1G125? How much is Maximum data rates in case of 5Vinput to 3.3Vout? We can't find it on the datasheet. Kind regards, Hirotaka Matsum…
Hellow Chris, Thank you for your reply.
I do not expect SN74CB3T1G125 to function correctly in such conditions. SN74CB3T1G125 pin B is connected to 1.8V tolerant FPGA pin so i have to decide whether to remove SN74CB3T1G125 or not from the board in order…
Part Number: SN74CB3T3125 Other Parts Discussed in Thread: SN74CB3T1G125 , SN74CB3T1G125-Q1 Hi,
Do you have any suggested part that is functionally compatible with SN74CB3T3125(4ch) and only support 1ch?
I’ve found SN74CB3T1G125(1ch) and SN74CB3T1G125…
Hi Hailiang,
As Clemens mentioned, this is a passive switch. As such the I/O's are not buffered. Please see this thread for more information.
(+) SN74CB3T1G125: IBIS model output configuration - Switches & multiplexers forum - Switches & multiplexers…
Part Number: SN74LVC2G66 Other Parts Discussed in Thread: SN74LVC1G66 , SN74CB3T1G125 , SN74CBTLV1G125 Hi team,
My customer is looking for an 1bit bidirectional automatic switch like I2C buffer. (They don't need a buffer function because it is unlikely…
Hi Adam,
Thank you for your reply.
I see the following application report about figure 10 and draw 5V pullup.
CBT series is near-zero propagation delay, so I didn't use LSF0101 or TXB0101.
I'd like to use bidirectional level shift circuit between…
Other Parts Discussed in Thread: SN74CB3T1G125 , SN74CB3T3245 Hello,
Can you look at the following datasheet discrepancy?
This is the functionality note for the single version of the CB3T family - SN74CB3T1G125:
NOTE A: If the input high voltage…