Part Number: SN74CB3T3306 The person running the simulation pointed out that there was no OUTPUT information in the IBIS model. Is there a file with output information?
If the file does not exist, I am thinking of setting temporary parameters. Is there…
Part Number: SN74CB3T3306 One of our Engineers has a question about the SN74CB3T3306DCUR. Would you please review and clarify?
Questions:
What is max ON-state resistance (ron) over operating free-air temperature range with Vcc = 3 V, Vi = 0.8 V…
Part Number: SN74CB3T3306 Other Parts Discussed in Thread: SN74CBT3383C Dear team,
My customer would like to replace 7WB383, onsemi device.
But our SN74CB3T3306 is only 2ch SPST. Is there any switch device to replace competitor device with below function…
Part Number: SN74CB3T3306 Other Parts Discussed in Thread: SN74LVC2G66 , SN74CB3Q3306A Hi
Customer has a question SN74CB3T3306 I want to use OE# to switch SMBUS, can both sides of A and B be +3.3V?
The schematic diagram is as follows: A and B are…
Part Number: SN74CB3Q3306A Please add the SN74CB3Q3306A and SN74CB3Q3306A-EP to your search page results, plus any other missing mux/switch parts. I just happened to run across the Q part, which is better for my application.
Part Number: SN74CB3T3306 Other Parts Discussed in Thread: LSF0102 Hello TI,
We are planning to use the voltage level translator (SN74CB3T3306) for conversion from +1.8V to +2.5V/+3.3V. And we do have Low Jitter Criteria for the signals that we are…
Part Number: SN74CB3T3306 Hi team,
My customer procured SN74CB3T3306DCTR. Top marking should be "WA6 Z" but it shown "WA6 81Z", please clarify.
Beat Regards, Tom Liu
Part Number: SN74CB3Q3306A Hello expert,
My customer would like to check why the EN signal for these two parts are the same but the function block are different. Could you kindly help to check on customer's question? Thanks a lot!
Best regards,
…
Part Number: SN74CB3T3306 Hello,
I am using the SN74CB3T3306DCUR to connect a 3.3V I/O to an signal that could be up to 5V. I need to be able to either receive a 3.3V or 5V signal OR transmit a 3.3V signal. I have this part's VCC connected to 3.3V and…
Part Number: SN74CB3T3306 Other Parts Discussed in Thread: SN74CBT3306 , , SN74CB3Q3306A e2e,
I'm using SN74CB3T3306DCTR , but found the B1 signal is reversed, the waveform as below.
I wonder does it happened in other project or do you have another…