Part Number: SN74LV4051A Tool/software: What is the reason for the EOL of the SN74LV4051APW?
We received back a defective product and traced the problem to a failure of two of the four SN74LV4051APW chips on our board. We see the part is now end-of-life…
Part Number: SN74LV4051A-Q1 Other Parts Discussed in Thread: SN74LV4051A Tool/software: Hi,
Q1) In DATASHEET_page 5_VIL, there are three lines with the expression "Vcc = 1.65V TO 2.7V". Is Vcc = 1.65V, Vcc = 2V, Vcc = 2.3V to 2.7V correct? There…
Part Number: SN74LV4051A Other Parts Discussed in Thread: CD74HCT4051 , TMUX4051 Hi team,
If VCC=5V, for high-logic level, can 3.3V work? Or it must be over 3.5V?
Thanks!
Rayna
Part Number: SN74LV4051A Hi team,
My customer wants to know what is the A,B,C pins current requirements and pull-up resistor's resistance limitation for SN74LV4051ADR ?
Thanks!
Best Regards,
Bowen
Part Number: SN74LV4051A
The RGY (16pin VQFN) package version of this part has a thermal pad. There is no indication on the datasheet if this pad should be bonded or not and if so to what. On the NXP equivalent to this part, they state the pad is not…
Part Number: SN74LV4051A Hi Team,
This is FAE Jayden. My customer used SN74LV4051ADR in their application.
Just want to check whether SN74LV4051ADR can be used for channel switching of UART communication?
Thanks
Brs
Jayden
Part Number: SN74LV4051A-Q1 Hi Experts,
Could you please recommend the proper R, Cap values or additional element for this schematic? (Pull-up R / Decoupling cap, etc)
Multiplexer IC SN74LV4051A-Q1
( VCC 5V / Input : LED cathode / Output & Chip Selector…
Part Number: SN74LV4051A-Q1 Dear expert, We will be using the SN74LV4051AQPWRQ1 IC for our project but we need below parameters:
Failure Mode Distribution
Pin FMEA
Can you provide parameters above?
Your help would be appreciated. Best regards, tatsuya…
Part Number: SN74LV4051A
Hi Expert,
Can you give us some advice of TI: SN74LV4051APWR
We have received the same PN but 2 different Xray images ..
Also there is dot on pin 1 of one sample while other sample with dimple? They both beloings to same TI part…