Part Number: SN74LV4T125-Q1 Hi Staff
SN74LV4T125-Q1
I am planning to mold SN74LV4T125-Q1, but is it possible to use it?
About molding agent Main agent: Pernox XN-2248 (clear) Hardening agent: Percure XY-2233-3 Epoxy filler, hardness 15
regards…
Part Number: SN74LV4T125-Q1 Other Parts Discussed in Thread: SN74LXC8T245-Q1 , TXU0204-Q1 Hi Team,
My customer is using the 74AVCH4T245PW-Q10J (TSSOP), however, it is max 3.6Vin, and are looking for 5.5Vin to translate from 5V to 1.8V.
I know we…
Part Number: TXU0304 Other Parts Discussed in Thread: TXB0104 , SN74LV4T125-Q1 Hi Team,
Since customer need to select device which has P2P backup device, could you please kindly help to check if we have P2P device with TXU0304 and SN74LV4T125PWR? And…
In total we are considering the following: Voltage translators & level shifters SN74AXC4T774-Q1 SN74AXC4T245-Q1 SN74AXC4T774 SN74AXCH4T245 SN74LV4T125 SN74AVC4T245-Q1 SN74AVCH4T245-EP SN74AVC4T774 SN74AXC4T245 SN74AVC4T245 SN74AVCH4T245 Buffers, drivers…
Part Number: ADC12DJ5200RFEVM Other Parts Discussed in Thread: LMX2594 , SN74LVC8T245 , TXV0108-Q1 , SN74LV4T125 , SN74LV1T126 Hi,
In ADC12DJ5200 EVAL board LMX2594 device inputs like CS, SCLK, SDI signals coming from FPGA are level translated to 3V3…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74LVC8T245 , , SN74LVC2T45 , SN74LVC16T245 , LSF0108-Q1 , TXB0108 , LSF0108 , SN74LV4T125 , CD40109B Hey Guys,
I made a terrible mistake: I use the SN74AXC8T245PW in my design and reconfigured…
Part Number: SN74LV4T125 Hi Team,
We understand that VOH is 4.4V(min) at VCC=5.0V, IOH=-16mA.
However, we would like to know Minimum VOH at VCC=5.0V and IOH= less than -16mA (so from 0mA to 15mA).
----------
[Q1]
Could you please let us…