Part Number: SN74LVC1G132 Hi TI Team,
Per PCN#20250731001.1 and PCN#20250731001.1A , Texas Instruments indicates the addition of manufacturing sites for SOT / SC70 devices. However, the PCNs do not clearly specify which assembly sites are currently…
Part Number: SN74LVC1G132 Hello,
I am using SN74LVC1G132 component in my design. I wanted to inquire about the failure condition of the SN74LVC1G132. What are the most common failure conditions and types for this components? Is there an failure analysis…
Part Number: SN74LVC1G132 Hello Technocrats,
Please provide junction-to-case thermal resistance data (Rjc) for the following parts,
1. SN74LVC1G132DBVR
2. OPA356AIDBVR
Part Number: SN74LVC1G132 Hello Technocrats,
Please provide junction-to-case thermal resistance data (Rjc) for the following parts,
1. SN74LVC1G132DBVR
2. OPA356AIDBVR
Part Number: SN74LVC1G132 Hi there, a customer is asking if SN74LVC1G132DBV has a bake at the during/end of assembly or before pack. What are the conditions (duration + temp) or is there a particular standard that is used?
Part Number: SN74LVC1G00 Other Parts Discussed in Thread: SN74LVC1G132 Hello TI Support,
We are using the SN74LVC1G00 at VCC = 3.3 V. The input is driven by an open-drain source with a fixed 1 kOhm pull-up resistor, and no additional external components…
Part Number: SN74HCS74 Other Parts Discussed in Thread: SN74LVC1G00 , SN74LVC1G132 Hi Logic Experts,
I'm using the sn74HCS74 to control power on/off. Below is my schematic.
The clock signal is drived by the output of the SN74LVC1G00。
Here is the…
Hi Ganesh,
This is for the whole device. We do not have a modern device that can drive 60 mA from the whole device. To get this drive I would split this into two separate SN74LVC1G132 .
Regards,
Owen
Hello Ryker,
Ryker She said: Could we connect the pin STEP1 and STEP2 with same frequency signal?
This would mean you'd start and stop the two steppers at the same time as well as run at the same speed or a multiple based on the microstep mode selection…