Part Number: AM26LS31 Other Parts Discussed in Thread: AM26LV31E , AM26C31 , AM26LV31 , SN74LVC2G66 , UCC27517 Tool/software: Hi TI E2E Team,
Good morning.
We (R&D Dynamics) are using " AM26LS31-Quadruple Differential Line Driver (PDF attached…
Part Number: TCA9543A Other Parts Discussed in Thread: TCA9546A , SN74LVC2G66 , SN74HCS74 , SN74LVC1G79 , SN74LVC1G175 Hi,
I would like to know if this is possible:
I think it is wrong because there is an address conflict, all TCA9543A have the same address…
The absolute maximum ratings forbid input voltages above V CC .
Use a comparator with shutdown function, or disconnect the inputs with a switch like the SN74LVC2G66.
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: SN74CBTLV3257 , , SN74LVC2G66-Q1 Hello. Can we have the Pspice model of the SN74LVC1G3157 and SN74CBTLV3257 devices?
HSpice can not be used with Tina nor Pspice TI tool!!
Regards.
Part Number: SN74LVC2G66 Hi Team,
We understand that ICC is 10uA(max) at VCC=5.5V, TA=-40℃ to 85℃ and ICC is 1uA(max) at VCC=5.5V, TA=25℃.
However, we would like to know about ICC value at VCC=1.9V, 3.8V, 5.0V and TA=-10℃ to 40℃.
Could you please let…
Part Number: SN74LVC2G66 Hello team ,
Can i used SN74LVC2G66 for I2c data line ?
i am asking because my i2c is open drain configuration with weak pullups to the 3.3V supply line .
Part Number: SN74LVC2G66 Hi Expert,
The customer reported the SN74LVC2G66 internal switch not functional well as expected on production project.
During applied high level to 1C pin.They customer see the internal switch (between 1A and 1B) not turn on…
Part Number: SN74LVC2G66-Q1 Other Parts Discussed in Thread: SN74LVC2G66 , TINA-TI Hi Champs,
My customer is looking for the I2C bus switch for automotive application.
If SN74LVC2G66 is used for I2C bus switch, is there any point to be taken care?
Customer…